<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: PF0200 - OTP Version Solo compatibility</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PF0200-OTP-Version-Solo-compatibility/m-p/663760#M101941</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Maximilian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at Table 1. Orderable Part Variations MMPF0200 Datasheet &lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2Fanalog%2Fdoc%2Fdata_sheet%2FMMPF0200.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0200.pdf&lt;/A&gt;&lt;BR /&gt;MMPF0200F6 is used on i.MX6SX SabreSD board&lt;BR /&gt;Schematics (1)&lt;BR /&gt;IMX6SOLOX-SABRESDB-DESIGNFILES&lt;BR /&gt;&lt;A href="http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-board-for-smart-devices-based-on-the-i.mx-6solox-applications-processors:RD-IMX6SX-SABRE?fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-board-for-smart-devices-based-on-the-i.mx-6solox-applications-processors:RD-IMX6SX-SABRE?fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Sep 2016 23:47:38 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-09-29T23:47:38Z</dc:date>
    <item>
      <title>PF0200 - OTP Version Solo compatibility</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0200-OTP-Version-Solo-compatibility/m-p/663759#M101940</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i want to supply a i.MX6-Solo-Design with DDR3L using a PF0200.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As far as i understand the power-up process (datasheet 4.2.1) i need to apply the VDD_SNVS_IN / VDD_HIGH_IN (which are connected in my design) first and can then power up the other supplys in any order.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So i think i may be able to use the F6 - OTP-Variant of the PF0200, if i connect:&lt;/P&gt;&lt;P&gt;- VGEN6_VOLT for&amp;nbsp;VDD_SNVS_IN / VDD_HIGH_IN (which is powered first)&lt;/P&gt;&lt;P&gt;- SW1 for core voltages (ARM; SOC) (order : 2)&lt;/P&gt;&lt;P&gt;- SW3 for Memory (order : 3)&lt;/P&gt;&lt;P&gt;- SW2 for IOs&amp;nbsp; (order : 4)&lt;/P&gt;&lt;P&gt;Is that correct?&lt;/P&gt;&lt;P&gt;Are there recommendation, which OTP-variant is suitable for which processor?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Sep 2016 14:24:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0200-OTP-Version-Solo-compatibility/m-p/663759#M101940</guid>
      <dc:creator>max123</dc:creator>
      <dc:date>2016-09-29T14:24:21Z</dc:date>
    </item>
    <item>
      <title>Re: PF0200 - OTP Version Solo compatibility</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0200-OTP-Version-Solo-compatibility/m-p/663760#M101941</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Maximilian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at Table 1. Orderable Part Variations MMPF0200 Datasheet &lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2Fanalog%2Fdoc%2Fdata_sheet%2FMMPF0200.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0200.pdf&lt;/A&gt;&lt;BR /&gt;MMPF0200F6 is used on i.MX6SX SabreSD board&lt;BR /&gt;Schematics (1)&lt;BR /&gt;IMX6SOLOX-SABRESDB-DESIGNFILES&lt;BR /&gt;&lt;A href="http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-board-for-smart-devices-based-on-the-i.mx-6solox-applications-processors:RD-IMX6SX-SABRE?fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-board-for-smart-devices-based-on-the-i.mx-6solox-applications-processors:RD-IMX6SX-SABRE?fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Sep 2016 23:47:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0200-OTP-Version-Solo-compatibility/m-p/663760#M101941</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-09-29T23:47:38Z</dc:date>
    </item>
  </channel>
</rss>