<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックAndroid 4.4.3 spdif out not working</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android-4-4-3-spdif-out-not-working/m-p/663452#M101851</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use android 4.4.3 and I would like use the Spidif out.&lt;/P&gt;&lt;P&gt;In ALSA device list imx-spdif is listed as audio card 1&lt;/P&gt;&lt;P&gt;I configured the /hardware/imx/alsa/config_spdif.h as out, after&lt;/P&gt;&lt;P&gt;I tried by console tinyplay /test.wav -D 1 -d 0.&lt;/P&gt;&lt;P&gt;I check by oscilloscope the out and it works, but I not listen sound.&lt;/P&gt;&lt;P&gt;It seems mute audio.&lt;/P&gt;&lt;P&gt;I tried by console tinyplay also with sgtl5000 and HDMI and sound is ok.&lt;/P&gt;&lt;P&gt;How can I check?&lt;/P&gt;&lt;P&gt;The Android 4.4.3 can transmit the spdif audio?&lt;/P&gt;&lt;P&gt;I not have error or warning in all logs, but I not have out sound.&lt;/P&gt;&lt;P&gt;Thanks in advance for any help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Sep 2016 09:16:49 GMT</pubDate>
    <dc:creator>marcobologna</dc:creator>
    <dc:date>2016-09-29T09:16:49Z</dc:date>
    <item>
      <title>Android 4.4.3 spdif out not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-4-4-3-spdif-out-not-working/m-p/663452#M101851</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use android 4.4.3 and I would like use the Spidif out.&lt;/P&gt;&lt;P&gt;In ALSA device list imx-spdif is listed as audio card 1&lt;/P&gt;&lt;P&gt;I configured the /hardware/imx/alsa/config_spdif.h as out, after&lt;/P&gt;&lt;P&gt;I tried by console tinyplay /test.wav -D 1 -d 0.&lt;/P&gt;&lt;P&gt;I check by oscilloscope the out and it works, but I not listen sound.&lt;/P&gt;&lt;P&gt;It seems mute audio.&lt;/P&gt;&lt;P&gt;I tried by console tinyplay also with sgtl5000 and HDMI and sound is ok.&lt;/P&gt;&lt;P&gt;How can I check?&lt;/P&gt;&lt;P&gt;The Android 4.4.3 can transmit the spdif audio?&lt;/P&gt;&lt;P&gt;I not have error or warning in all logs, but I not have out sound.&lt;/P&gt;&lt;P&gt;Thanks in advance for any help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Sep 2016 09:16:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-4-4-3-spdif-out-not-working/m-p/663452#M101851</guid>
      <dc:creator>marcobologna</dc:creator>
      <dc:date>2016-09-29T09:16:49Z</dc:date>
    </item>
    <item>
      <title>Re: Android 4.4.3 spdif out not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-4-4-3-spdif-out-not-working/m-p/663453#M101852</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marco&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can test with linux, please check sect.32.2 S/PDIF Tx Driver attached&lt;/P&gt;&lt;P&gt;Linux Manual, use nxp Linux 3.10.53 bsp&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/webapp/Download?colCode=L3.10.53_1.1.0_iMX6QDLS_Bundle&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product" title="http://www.nxp.com/webapp/Download?colCode=L3.10.53_1.1.0_iMX6QDLS_Bundle&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product"&gt;http://www.nxp.com/webapp/Download?colCode=L3.10.53_1.1.0_iMX6QDLS_Bundle&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=13…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Sep 2016 11:33:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-4-4-3-spdif-out-not-working/m-p/663453#M101852</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-09-30T11:33:24Z</dc:date>
    </item>
    <item>
      <title>Re: Android 4.4.3 spdif out not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-4-4-3-spdif-out-not-working/m-p/663454#M101853</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem was solved!!!!&lt;/P&gt;&lt;P&gt;The bit SCR_VAL_CLEAR to register SPDIF_SCR and is mask must be set to work..&lt;/P&gt;&lt;P&gt;The "validity" flag (bit 28 in each subframe, counting from preamble bit 0) was going out as 1 rather than 0, and per SP-DIF standard '1' denotes an *invalid* sample, like from a scratched CD giving read errors (though it's reversed again in i.MX6 SPDIF_SCR register, where the power-on default '0' in bit 5 means "send out 1s").&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/kernel_imx/sound/soc/fsl/fsl_spdif.c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if (substream-&amp;gt;stream == SNDRV_PCM_STREAM_PLAYBACK) {&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;scr = SCR_TXFIFO_AUTOSYNC | SCR_TXFIFO_CTRL_NORMAL |&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;SCR_TXSEL_NORMAL | SCR_USRC_SEL_CHIP |&lt;BR /&gt; -&amp;nbsp;&amp;nbsp;&amp;nbsp;SCR_TXFIFO_FSEL_IF8;&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp;SCR_TXFIFO_FSEL_IF8 | SCR_VAL_CLEAR;&lt;BR /&gt; &lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;mask = SCR_TXFIFO_AUTOSYNC_MASK | SCR_TXFIFO_CTRL_MASK |&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;SCR_TXSEL_MASK | SCR_USRC_SEL_MASK |&lt;BR /&gt; -&amp;nbsp;&amp;nbsp;&amp;nbsp;SCR_TXFIFO_FSEL_MASK;&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp;SCR_TXFIFO_FSEL_MASK | SCR_VAL_MASK;&lt;BR /&gt; &lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;for (i = 0; i &amp;lt; SPDIF_TXRATE_MAX; i++) &lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;clk_prepare_enable(spdif_priv-&amp;gt;txclk[i]);&lt;BR /&gt; &lt;BR /&gt; } &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Sep 2016 17:42:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-4-4-3-spdif-out-not-working/m-p/663454#M101853</guid>
      <dc:creator>marcobologna</dc:creator>
      <dc:date>2016-09-30T17:42:38Z</dc:date>
    </item>
  </channel>
</rss>