<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.MX6 Linux usage of OCRAM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Linux-usage-of-OCRAM/m-p/662299#M101685</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vincent&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for memory usage please refer to Chapter 3 Machine Specific Layer (MSL)&lt;/P&gt;&lt;P&gt;attached Linux Manual. Yes Linux uses the OCRAM, i.MX6Q OCRAM is 256 KB,&lt;/P&gt;&lt;P&gt;"alias" means the same memory mapped on other address.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Jan 2017 03:58:59 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-01-06T03:58:59Z</dc:date>
    <item>
      <title>i.MX6 Linux usage of OCRAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Linux-usage-of-OCRAM/m-p/662298#M101684</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi !&lt;/P&gt;&lt;P&gt;We are running a secure OS alongside Linux on some different flavors of i.MX6 boards, and we need to use the OCRAM from the Secure Side. I want to protect the code/data we put on the OCRAM using the provided OCRAM_TZASC. But I am not 100% sure about some behavior of Linux:&lt;/P&gt;&lt;P&gt;* Is Linux using the OCRAM at all ? (maybe for some low power/ suspend features ?)&lt;/P&gt;&lt;P&gt;* If Linux is using the OCRAM, where can I find this in the code, so I can survey how much memory is needed, and I can put our secure information in a different location, so we don't fight over memory&lt;/P&gt;&lt;P&gt;* Is the total amount of OCRAM is 256 Kb ? I'm not sure about the "OCRAM aliased" entry in the memory table.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For your information, we are using 2 flavors of Linux:&lt;/P&gt;&lt;P&gt;* one from NXP: git://git.freescale.com/imx/linux-2.6-imx.git&lt;/P&gt;&lt;P&gt;* one from Boundary Devices (for our sabre lite boards): git://github.com/boundarydevices/linux-imx6.git&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;V.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jan 2017 08:24:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Linux-usage-of-OCRAM/m-p/662298#M101684</guid>
      <dc:creator>vsiles</dc:creator>
      <dc:date>2017-01-05T08:24:00Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 Linux usage of OCRAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Linux-usage-of-OCRAM/m-p/662299#M101685</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vincent&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for memory usage please refer to Chapter 3 Machine Specific Layer (MSL)&lt;/P&gt;&lt;P&gt;attached Linux Manual. Yes Linux uses the OCRAM, i.MX6Q OCRAM is 256 KB,&lt;/P&gt;&lt;P&gt;"alias" means the same memory mapped on other address.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jan 2017 03:58:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Linux-usage-of-OCRAM/m-p/662299#M101685</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-01-06T03:58:59Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 Linux usage of OCRAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Linux-usage-of-OCRAM/m-p/662300#M101686</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi !&lt;/P&gt;&lt;P&gt;Thank you for the document, it gave me hints on which file to parse. I'll try to see how much OCRAM linux is using, so I can reserve some for secure usage.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jan 2017 08:13:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Linux-usage-of-OCRAM/m-p/662300#M101686</guid>
      <dc:creator>vsiles</dc:creator>
      <dc:date>2017-01-06T08:13:37Z</dc:date>
    </item>
  </channel>
</rss>