<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Uncompressing Linux... done, booting the kernel. stoped after this. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Uncompressing-Linux-done-booting-the-kernel-stoped-after-this/m-p/662050#M101654</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sagar&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Uncompressing Linux... hanging may mean ddr errors, so one can try ddr test&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://community.freescale.com/docs/DOC-105652" title="https://community.freescale.com/docs/DOC-105652"&gt;https://community.freescale.com/docs/DOC-105652&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and rebuild uboot with new calibration coefficients placed in uboot/../mx6qsabresd/*.cfg file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Feb 2017 01:06:33 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-02-24T01:06:33Z</dc:date>
    <item>
      <title>Uncompressing Linux... done, booting the kernel. stoped after this.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uncompressing-Linux-done-booting-the-kernel-stoped-after-this/m-p/662049#M101653</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to boot the kernel through sd card, and sticking into following problem:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;MX6Q CAMARO U-Boot &amp;gt; source boot&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;## Executing script at 0000000b&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;data abort&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;MAYBE you should read doc/README.arm-unaligned-accesses&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;pc : [&amp;lt;2ff8faac&amp;gt;] lr : [&amp;lt;2ff88fac&amp;gt;]&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;sp : 2fcffe10 ip : 00000000 fp : 2fd00dd8&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;r10: 2ffbab1c r9 : 00000002 r8 : 2fcfff38&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;r7 : 2fd00de8 r6 : 00000000 r5 : ffffffff r4 : 0000000b&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;r3 : 00000001 r2 : 00000003 r1 : 00000080 r0 : 0000000b&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Flags: nZCv IRQs off FIQs off Mode SVC_32&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Resetting CPU ...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;resetting ...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;EM&gt;U-Boot 2013.07 (Oct 07 2015 - 09:37:17)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;CPU: Freescale i.MX6Q rev1.2 at 792 MHz&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Reset cause: WDOG&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Board: MX6Q-Camaro&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;DRAM: 512 MiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Failed to probe i2c&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;failed to read lcd board ID&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;SF: Detected S25FL512SA with page size 64 KiB, total 64 MiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Display: OT43 (480x800)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Loading splashimage into 0x13000000...&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;** File not found splash.bmp **&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;** File not found splash.bmp **&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Framebuffer at 0x2fd43698&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Error: no valid bmp image at 13000000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;In: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Out: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Err: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;SF: Detected S25FL512SA with page size 64 KiB, total 64 MiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;bootAttempts=4&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Net: FEC&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Warning: failed to set MAC address&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Hit any key to stop autoboot: 0 &lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mmc0 is current device&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mmc0 is current device&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;** Unrecognized filesystem type **&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Failed to mount ext2 filesystem...&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;** Unrecognized filesystem type **&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Failed to mount ext2 filesystem...&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;** Unrecognized filesystem type **&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;3576968 bytes read in 314 ms (10.9 MiB/s)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Booting from mmc ...&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;## Booting kernel from Legacy Image at 80800000 ...&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; Image Name: Linux-3.0.35&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; Image Type: ARM Linux Kernel Image (uncompressed)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; Data Size: 3576904 Bytes = 3.4 MiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; Load Address: 80008000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; Entry Point: 80008000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; Verifying Checksum ... OK&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; Loading Kernel Image ... OK&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Starting kernel ...&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Uncompressing Linux... done, booting the kernel.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The u-boot environment parameters are as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;MX6Q CAMARO U-Boot &amp;gt; printenv&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;baudrate=115200&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;bootAttempts=5&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;bootargs=console=ttymxc1,115200 root=/dev/nfs ip=dhcp nfsroot=:,v3,tcp&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;bootcmd=mmc dev ${mmcdev};mmc dev ${mmcdev}; if mmc rescan; then if run loadbootscript; then run bootscript; else if run loaduimage; then run mmcboot; else run netboot;fi;fi;fi&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;bootdelay=3&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;bootdelay3&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;bootscript=echo Running bootscript from mmc ...; source&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;clearnenv=sf probe; sf erase 0x100000 0x140000&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;console=ttymxc1&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;cpuId=1&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;cpuRevision=2&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;ethact=FEC&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;fdt_high=0xffffffff&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;filesize=369488&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;findTag=for part in 0 1;do ext2load mmc 0:${part} 80008000 thermoboot&amp;amp;&amp;amp; source 80008000; done&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;flash_uboot=echo flashing U-Boot from ${loadaddr}...; sf probe; sf erase 0 0x40000; sf write ${loadaddr} 0x400 0x40000&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;initaddr=0x11000000&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;initrd_high=0xffffffff&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;kernel=uImage&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;lcdId=0&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;lcdRevision=0&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;load_splashimage=echo Loading splashimage into ${splashimage}...; mmc rescan; if ext2load mmc 0:2 ${splashimage} splash.bmp; then echo "------ loaded splash from normal partition"; else;ext2load mmc 0:1 ${splashimage} splash.bmp; fi&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;load_uboot=echo loading U-Boot to ${loadaddr} from mmc...; mmc rescan; ext2load mmc ${mmcdev}:${mmcpart} ${loadaddr} u-boot.imx&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;loadaddr=0x80800000&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;loaduimage=run findTag;ext2load mmc ${mmcdev}:${mmcpart} ${loadaddr} ${uimage}&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;mmcargs=setenv bootargs console=ttymxc1,115200 consoleblank=0 root=/dev/mmcblk0p1 rootwait rw xl4&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;mmcboot=echo Booting from mmc ...; run mmcargs; bootm&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;mmcdev=0&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;mmcpart=1&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;mmcroot=/dev/mmcblk0p1 rootwait rw&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;netargs=setenv bootargs console=${console},${baudrate} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;netboot=echo Booting from net ...; run netargs; dhcp ${uimage}; bootm&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;part=0&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;platId=0&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;recovery_mode=1&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;script=boot.scr&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;splashimage=0x13000000&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;stderr=serial&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;stdin=serial&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;stdout=serial&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;uimage=boot/uImage&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;upgrade_uboot=run load_uboot flash_uboot&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;video=mxcfb0:dev=lcd,OT27,if=RGB666 video=mxcfb1:off&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Environment size: 2020/262140 bytes&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;MX6Q CAMARO U-Boot &amp;gt;&lt;/STRONG&gt; &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is there any mistake in u-boot environment setting, or something else??&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Feb 2017 09:19:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uncompressing-Linux-done-booting-the-kernel-stoped-after-this/m-p/662049#M101653</guid>
      <dc:creator>sagarojha</dc:creator>
      <dc:date>2017-02-23T09:19:54Z</dc:date>
    </item>
    <item>
      <title>Re: Uncompressing Linux... done, booting the kernel. stoped after this.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uncompressing-Linux-done-booting-the-kernel-stoped-after-this/m-p/662050#M101654</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sagar&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Uncompressing Linux... hanging may mean ddr errors, so one can try ddr test&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://community.freescale.com/docs/DOC-105652" title="https://community.freescale.com/docs/DOC-105652"&gt;https://community.freescale.com/docs/DOC-105652&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and rebuild uboot with new calibration coefficients placed in uboot/../mx6qsabresd/*.cfg file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Feb 2017 01:06:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uncompressing-Linux-done-booting-the-kernel-stoped-after-this/m-p/662050#M101654</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-02-24T01:06:33Z</dc:date>
    </item>
  </channel>
</rss>