<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimxcompositor_g2d and imxv4l2src problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imxcompositor-g2d-and-imxv4l2src-problem/m-p/662017#M101644</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;when trying to combine a picture and video (using &amp;nbsp;imxv4l2src ) using the&amp;nbsp;imxcompositor_g2d we get very poor framerate. 5% resources are shown with "top".&lt;/P&gt;&lt;P&gt;using the same pipeline while using a filesrc (video) instead, the framerate is as expected with the same resources used.&lt;/P&gt;&lt;P&gt;The only reason I could see is that the camera source outputs the frame in interlace-mode=interleaved, which seemingly is not supported by the&amp;nbsp;&lt;SPAN&gt;imxcompositor_g2d.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When connecting the same camera source to the sink element, the video looks perfect.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The input to the camera interface is UYVY 1280X720 16bit interface.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;GStreamer Core Library version 1.4.5&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Linux imx6qsabresd 3.14.52-g29edc48-dirty&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Feb 2017 14:02:23 GMT</pubDate>
    <dc:creator>reuelhaavrahami</dc:creator>
    <dc:date>2017-02-01T14:02:23Z</dc:date>
    <item>
      <title>imxcompositor_g2d and imxv4l2src problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imxcompositor-g2d-and-imxv4l2src-problem/m-p/662017#M101644</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;when trying to combine a picture and video (using &amp;nbsp;imxv4l2src ) using the&amp;nbsp;imxcompositor_g2d we get very poor framerate. 5% resources are shown with "top".&lt;/P&gt;&lt;P&gt;using the same pipeline while using a filesrc (video) instead, the framerate is as expected with the same resources used.&lt;/P&gt;&lt;P&gt;The only reason I could see is that the camera source outputs the frame in interlace-mode=interleaved, which seemingly is not supported by the&amp;nbsp;&lt;SPAN&gt;imxcompositor_g2d.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When connecting the same camera source to the sink element, the video looks perfect.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The input to the camera interface is UYVY 1280X720 16bit interface.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;GStreamer Core Library version 1.4.5&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Linux imx6qsabresd 3.14.52-g29edc48-dirty&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Feb 2017 14:02:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imxcompositor-g2d-and-imxv4l2src-problem/m-p/662017#M101644</guid>
      <dc:creator>reuelhaavrahami</dc:creator>
      <dc:date>2017-02-01T14:02:23Z</dc:date>
    </item>
    <item>
      <title>Re: imxcompositor_g2d and imxv4l2src problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imxcompositor-g2d-and-imxv4l2src-problem/m-p/662018#M101645</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Reuel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please try procedures given in sect.7.3.16 Video composition&lt;/P&gt;&lt;P&gt;sect.7.3.15 Video conversion attached Linux Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Feb 2017 03:20:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imxcompositor-g2d-and-imxv4l2src-problem/m-p/662018#M101645</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-02-02T03:20:57Z</dc:date>
    </item>
    <item>
      <title>Re: imxcompositor_g2d and imxv4l2src problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imxcompositor-g2d-and-imxv4l2src-problem/m-p/662019#M101646</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I looked at the document. using fake sources and file sources works fine and I can see the expected frame rate, but using the imxv4l2src does not work. The output on running the pipeline shows the following&lt;/P&gt;&lt;P&gt;WARNING: from element /GstPipeline:pipeline0/GstImxV4l2Sink:imxv4l2sink0: A lot of buffers are being dropped.&lt;BR /&gt;Additional debug info:&lt;BR /&gt;/home/haggay/workspace/FrameBuffer/fsl-release-bsp/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer1.0/1.4.5-r0/gstreamer-1.4.5/libs/gst/base/gstbasesink.c(2794): gst_base_sink_is_too_late (): /GstPipeline:pipeline0/GstImxV4l2Sink:imxv4l2sink0:&lt;BR /&gt;There may be a timestamping problem, or this computer is too slow.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Feb 2017 14:23:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imxcompositor-g2d-and-imxv4l2src-problem/m-p/662019#M101646</guid>
      <dc:creator>reuelhaavrahami</dc:creator>
      <dc:date>2017-02-02T14:23:50Z</dc:date>
    </item>
  </channel>
</rss>