<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX6UL USB over current functionality</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-USB-over-current-functionality/m-p/661852#M101612</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;See&amp;nbsp;&lt;A href="https://community.nxp.com/thread/438911"&gt;https://community.nxp.com/thread/438911&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Nov 2016 11:52:59 GMT</pubDate>
    <dc:creator>RossMcLuckie</dc:creator>
    <dc:date>2016-11-15T11:52:59Z</dc:date>
    <item>
      <title>iMX6UL USB over current functionality</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-USB-over-current-functionality/m-p/661851#M101611</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using the iMX6UL as a USB host controller, with an external power switch with over current status.&lt;/P&gt;&lt;P&gt;If I wire the OC status to a iMX6UL OC pin (as described in table 54-1 of the iMX6UL Reference Manual). Will there be any HW dependencies when a OC situation occurs:&lt;/P&gt;&lt;P&gt;1: Activating the OC input, will the USB data transfer be interrupted?&lt;/P&gt;&lt;P&gt;2: Will the OC input by any means directly control the PWR output?&lt;/P&gt;&lt;P&gt;I am thinking of any HW links between functions of the USB block.&lt;/P&gt;&lt;P&gt;A lot of reference designs are using any other GPIO pin for OC status, which I assume requires the USB driver to be adapted to that. But as the Reference Manual lists a number of dedicated pins for OC status, I'm wondering if the chip itself has any HW functionality for handling OC situations.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Nov 2016 09:19:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-USB-over-current-functionality/m-p/661851#M101611</guid>
      <dc:creator>hansjpetersen</dc:creator>
      <dc:date>2016-11-15T09:19:52Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6UL USB over current functionality</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-USB-over-current-functionality/m-p/661852#M101612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;See&amp;nbsp;&lt;A href="https://community.nxp.com/thread/438911"&gt;https://community.nxp.com/thread/438911&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Nov 2016 11:52:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-USB-over-current-functionality/m-p/661852#M101612</guid>
      <dc:creator>RossMcLuckie</dc:creator>
      <dc:date>2016-11-15T11:52:59Z</dc:date>
    </item>
  </channel>
</rss>