<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Forcing i.MX6 USB Host controller to Full-speed in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Forcing-i-MX6-USB-Host-controller-to-Full-speed/m-p/661627#M101577</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The discussions are around limiting i.MX6 USB device controller (Chipidea) to Full-speed. I am looking for methods to limit speed of host controller usb_h1 to Full speed if it is possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ganesan. K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Dec 2016 08:49:29 GMT</pubDate>
    <dc:creator>ganesank</dc:creator>
    <dc:date>2016-12-14T08:49:29Z</dc:date>
    <item>
      <title>Forcing i.MX6 USB Host controller to Full-speed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Forcing-i-MX6-USB-Host-controller-to-Full-speed/m-p/661625#M101575</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to force i.MX6 host-controller to act like Full-speed host controller supporting only full-speed devices downstream in Linux? If so please share the details. We are facing ESD &amp;amp; EFT issues in our product which seems to reduce with full speed USB topology.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using Yocto 2.1 - Linux 4.1 with our custom board based on Advantech Q7 i.MX6D module.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 10:51:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Forcing-i-MX6-USB-Host-controller-to-Full-speed/m-p/661625#M101575</guid>
      <dc:creator>ganesank</dc:creator>
      <dc:date>2016-12-09T10:51:28Z</dc:date>
    </item>
    <item>
      <title>Re: Forcing i.MX6 USB Host controller to Full-speed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Forcing-i-MX6-USB-Host-controller-to-Full-speed/m-p/661626#M101576</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ganesan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/343675"&gt;https://community.nxp.com/thread/343675&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 23:52:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Forcing-i-MX6-USB-Host-controller-to-Full-speed/m-p/661626#M101576</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-12-09T23:52:42Z</dc:date>
    </item>
    <item>
      <title>Re: Forcing i.MX6 USB Host controller to Full-speed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Forcing-i-MX6-USB-Host-controller-to-Full-speed/m-p/661627#M101577</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The discussions are around limiting i.MX6 USB device controller (Chipidea) to Full-speed. I am looking for methods to limit speed of host controller usb_h1 to Full speed if it is possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ganesan. K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 08:49:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Forcing-i-MX6-USB-Host-controller-to-Full-speed/m-p/661627#M101577</guid>
      <dc:creator>ganesank</dc:creator>
      <dc:date>2016-12-14T08:49:29Z</dc:date>
    </item>
    <item>
      <title>Re: Forcing i.MX6 USB Host controller to Full-speed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Forcing-i-MX6-USB-Host-controller-to-Full-speed/m-p/661628#M101578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ganesan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;solution is the same for host&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 08:53:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Forcing-i-MX6-USB-Host-controller-to-Full-speed/m-p/661628#M101578</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-12-14T08:53:40Z</dc:date>
    </item>
    <item>
      <title>Re: Forcing i.MX6 USB Host controller to Full-speed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Forcing-i-MX6-USB-Host-controller-to-Full-speed/m-p/661629#M101579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ganesan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you found out to limit the USB bus speed to full speed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/Igor1z"&gt;Igor1z&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;Can you please help us to limit the USB bus speed to full speed only on i.mx6ul linux&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 09:36:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Forcing-i-MX6-USB-Host-controller-to-Full-speed/m-p/661629#M101579</guid>
      <dc:creator>dhvanil_patel1</dc:creator>
      <dc:date>2017-02-07T09:36:13Z</dc:date>
    </item>
    <item>
      <title>Re: Forcing i.MX6 USB Host controller to Full-speed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Forcing-i-MX6-USB-Host-controller-to-Full-speed/m-p/661630#M101580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Patel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are using 4.1.x kernel then it is very straightforward. For forcing host controller to full-speed just add one line&amp;nbsp;&amp;nbsp;&lt;EM&gt;maximum-speed = "full-speed"; &amp;nbsp;&lt;/EM&gt;for the concerned host controller section in&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;your device tree (.dts) file. For example, see my settings for host controller 1 (usbh1)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;amp;usbh1 {&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;vbus-supply = &amp;lt;&amp;amp;reg_usb_h1_vbus&amp;gt;;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;reset-gpios = &amp;lt;&amp;amp;gpio7 11 0&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;STRONG&gt;&amp;nbsp;maximum-speed = "full-speed";&lt;/STRONG&gt;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;status = "okay";&lt;BR /&gt; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This approach works for OTG as well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Feb 2017 10:24:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Forcing-i-MX6-USB-Host-controller-to-Full-speed/m-p/661630#M101580</guid>
      <dc:creator>ganesank</dc:creator>
      <dc:date>2017-02-10T10:24:55Z</dc:date>
    </item>
  </channel>
</rss>