<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX6Q Boot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Boot/m-p/661143#M101500</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have custom developed i.MX6Q based SOM. In this we are observing following behaviour in boot media selection:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Boot pins are set to mSD and mSD is not inserted, then Boot loader will boot from SPI-NOR Flash.&lt;/LI&gt;&lt;LI&gt;Boot pins are set to mSD and mSD is present, Boot loader will boot from mSD.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Is this the expected behaviour, to boot from SPI-NOR flash if the selected boot media is not present?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below is the i.MX6Q processor part number we are using:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;MCIMX6Q5EYM12AD&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With Regards,&lt;/P&gt;&lt;P&gt;Vishakh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Sep 2016 06:00:28 GMT</pubDate>
    <dc:creator>vishakh</dc:creator>
    <dc:date>2016-09-29T06:00:28Z</dc:date>
    <item>
      <title>i.MX6Q Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Boot/m-p/661143#M101500</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have custom developed i.MX6Q based SOM. In this we are observing following behaviour in boot media selection:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Boot pins are set to mSD and mSD is not inserted, then Boot loader will boot from SPI-NOR Flash.&lt;/LI&gt;&lt;LI&gt;Boot pins are set to mSD and mSD is present, Boot loader will boot from mSD.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Is this the expected behaviour, to boot from SPI-NOR flash if the selected boot media is not present?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below is the i.MX6Q processor part number we are using:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;MCIMX6Q5EYM12AD&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With Regards,&lt;/P&gt;&lt;P&gt;Vishakh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Sep 2016 06:00:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Boot/m-p/661143#M101500</guid>
      <dc:creator>vishakh</dc:creator>
      <dc:date>2016-09-29T06:00:28Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6Q Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Boot/m-p/661144#M101501</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, this is not the expected behaviour.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Sep 2016 11:53:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Boot/m-p/661144#M101501</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-09-29T11:53:42Z</dc:date>
    </item>
  </channel>
</rss>