<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Booting 4.1.15 device tree  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Booting-4-1-15-device-tree/m-p/660758#M101416</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Most likely, your custom .dtb file is either wrong, corrupted or located in the wrong place. Please check. Also, refer to the attached document.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Nov 2016 11:34:32 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2016-11-29T11:34:32Z</dc:date>
    <item>
      <title>Booting 4.1.15 device tree</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-4-1-15-device-tree/m-p/660757#M101415</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am finding some difficulty in booting 4.1.15 kernel with customized device tree for sabresd board. The issue is, when device tree is loading there is a hang.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below are the logs,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0 is current device&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;6616512 bytes read in 328 ms (19.2 MiB/s)&lt;BR /&gt;reading imx6qp-sabresd.dtb&lt;BR /&gt;47155 bytes read in 20 ms (2.2 MiB/s)&lt;BR /&gt;## Booting kernel from Legacy Image at 12000000 ...&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Image Name:&amp;nbsp;&amp;nbsp; Linux-4.1.15-svn443&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Image Type:&amp;nbsp;&amp;nbsp; ARM Linux Kernel Image (uncompressed)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 6616448 Bytes = 6.3 MiB&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Load Address: 10008000&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Entry Point:&amp;nbsp; 10008000&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Verifying Checksum ... OK&lt;BR /&gt;## Flattened Device Tree blob at 18000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Booting using the fdt blob at 0x18000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Loading Kernel Image ... OK&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Using Device Tree in place at 18000000, end 1800e832&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The bootcmd is&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;setenv bootcmd 'mmc dev 0;fatload mmc 0 0x12000000 uImage;fatload mmc 0 0x18000000 imx6qp-sabresd.dtb;bootm 0x12000000 - 0x18000000'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The important thing is, board has quad plus i.mx6 processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Nov 2016 05:32:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-4-1-15-device-tree/m-p/660757#M101415</guid>
      <dc:creator>manjunathjoshi</dc:creator>
      <dc:date>2016-11-15T05:32:16Z</dc:date>
    </item>
    <item>
      <title>Re: Booting 4.1.15 device tree</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-4-1-15-device-tree/m-p/660758#M101416</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Most likely, your custom .dtb file is either wrong, corrupted or located in the wrong place. Please check. Also, refer to the attached document.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Nov 2016 11:34:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-4-1-15-device-tree/m-p/660758#M101416</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-11-29T11:34:32Z</dc:date>
    </item>
    <item>
      <title>Re: Booting 4.1.15 device tree</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-4-1-15-device-tree/m-p/660759#M101417</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Artur,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The issue is solved with&lt;/P&gt;&lt;P&gt;1. Proper calibration of DDR&lt;/P&gt;&lt;P&gt;2. Using proper bootargs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 06:13:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-4-1-15-device-tree/m-p/660759#M101417</guid>
      <dc:creator>manjunathjoshi</dc:creator>
      <dc:date>2016-12-14T06:13:24Z</dc:date>
    </item>
    <item>
      <title>Re: Booting 4.1.15 device tree</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-4-1-15-device-tree/m-p/660760#M101418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manjunath,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Coud you please explain how you did exactly? I got similar problem. :smileysad:&lt;BR /&gt;Thanks a lot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Raimund&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jun 2017 10:32:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-4-1-15-device-tree/m-p/660760#M101418</guid>
      <dc:creator>raimundszabo</dc:creator>
      <dc:date>2017-06-12T10:32:51Z</dc:date>
    </item>
  </channel>
</rss>