<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6DQ audio interface. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-audio-interface/m-p/660533#M101369</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SSI and ESAI work independently from each other an may be used&lt;/P&gt;&lt;P&gt;together. There are no restricitions on number of audio interfaces (SSI + ESAI).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Sep 2016 10:02:21 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-09-28T10:02:21Z</dc:date>
    <item>
      <title>i.MX6DQ audio interface.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-audio-interface/m-p/660532#M101368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about i.MX6DQ audio interface.&lt;BR /&gt;Actually, our customer have used 3 audio inputs/outputs with SSI1 to SSI3.&lt;BR /&gt;In this case, can they add a new audio input/output with ESAI?&lt;/P&gt;&lt;P&gt;Would you let me know what is the maximum number of audio interface (SSI + ESAI) i.MX6DQ can be used?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Sep 2016 09:09:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-audio-interface/m-p/660532#M101368</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2016-09-28T09:09:40Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6DQ audio interface.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-audio-interface/m-p/660533#M101369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SSI and ESAI work independently from each other an may be used&lt;/P&gt;&lt;P&gt;together. There are no restricitions on number of audio interfaces (SSI + ESAI).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Sep 2016 10:02:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-audio-interface/m-p/660533#M101369</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-09-28T10:02:21Z</dc:date>
    </item>
  </channel>
</rss>