<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: PMIC can't be found</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-can-t-be-found/m-p/660469#M101354</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Golan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can remove all pmic references in uboot sources,&lt;/P&gt;&lt;P&gt;like power_init_board() in uboot/board/freescale/mx6sabresd/mx6sabresd.c.&lt;/P&gt;&lt;P&gt;Also may be useful to check attached Porting Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 09 Apr 2017 23:18:10 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-04-09T23:18:10Z</dc:date>
    <item>
      <title>PMIC can't be found</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-can-t-be-found/m-p/660468#M101353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to run u-boot on my IMX6s, I'm using "mx6qpsabresd_defconfig" to configure it.&lt;/P&gt;&lt;P&gt;When I insert the sd card into the board, it start loading and then I see the next error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can't find PMIC:PFUZE100&lt;BR /&gt;initcall sequence 4ff96994 failed at call 1780429c (err=-19)&lt;BR /&gt;### ERROR ### Please RESET the board ###&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The board is modified, it has no PMIC module, instead I'm using fixed voltage which I can't control using the I2C.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I configure the u-boot not to look for PMIC?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 09 Apr 2017 16:01:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-can-t-be-found/m-p/660468#M101353</guid>
      <dc:creator>golansabo</dc:creator>
      <dc:date>2017-04-09T16:01:06Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC can't be found</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-can-t-be-found/m-p/660469#M101354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Golan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can remove all pmic references in uboot sources,&lt;/P&gt;&lt;P&gt;like power_init_board() in uboot/board/freescale/mx6sabresd/mx6sabresd.c.&lt;/P&gt;&lt;P&gt;Also may be useful to check attached Porting Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 09 Apr 2017 23:18:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-can-t-be-found/m-p/660469#M101354</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-04-09T23:18:10Z</dc:date>
    </item>
  </channel>
</rss>