<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: WiFi chipset supporting AP mode</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-chipset-supporting-AP-mode/m-p/660348#M101338</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jaffin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;L3.14.xx early versions supported Atheros AR6003 please refer to attached&lt;/P&gt;&lt;P&gt;Linux Manual Chapter 48 AR6003 WiFi.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/webapp/Download?colCode=L3.14.28_1.0.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product" title="http://www.nxp.com/webapp/Download?colCode=L3.14.28_1.0.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product"&gt;http://www.nxp.com/webapp/Download?colCode=L3.14.28_1.0.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageTyp…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;for broadcom wifi options one can check&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://wikidevi.com/wiki/Broadcom#USB" title="https://wikidevi.com/wiki/Broadcom#USB"&gt;https://wikidevi.com/wiki/Broadcom#USB&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Jan 2017 06:54:54 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-01-05T06:54:54Z</dc:date>
    <item>
      <title>WiFi chipset supporting AP mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-chipset-supporting-AP-mode/m-p/660347#M101337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am in search of a Wifi chipset which can be interfaced with iMX6 QuadPlus Sabre board easily (I am running linux 3.14) and which supports dual band frequency and AP mode and has a good performance. I have found BCM4330 chipset. Is there any other better option. Also is there any USB adapter with BCM4330 to connect with the board and test it out before buying the chipset. Any information regarding this will be helpful.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jan 2017 15:51:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WiFi-chipset-supporting-AP-mode/m-p/660347#M101337</guid>
      <dc:creator>jaffinmk</dc:creator>
      <dc:date>2017-01-04T15:51:02Z</dc:date>
    </item>
    <item>
      <title>Re: WiFi chipset supporting AP mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-chipset-supporting-AP-mode/m-p/660348#M101338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jaffin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;L3.14.xx early versions supported Atheros AR6003 please refer to attached&lt;/P&gt;&lt;P&gt;Linux Manual Chapter 48 AR6003 WiFi.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/webapp/Download?colCode=L3.14.28_1.0.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product" title="http://www.nxp.com/webapp/Download?colCode=L3.14.28_1.0.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product"&gt;http://www.nxp.com/webapp/Download?colCode=L3.14.28_1.0.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageTyp…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;for broadcom wifi options one can check&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://wikidevi.com/wiki/Broadcom#USB" title="https://wikidevi.com/wiki/Broadcom#USB"&gt;https://wikidevi.com/wiki/Broadcom#USB&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jan 2017 06:54:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WiFi-chipset-supporting-AP-mode/m-p/660348#M101338</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-01-05T06:54:54Z</dc:date>
    </item>
  </channel>
</rss>