<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックHow uboot can be written over NOR Flash using UART</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-uboot-can-be-written-over-NOR-Flash-using-UART/m-p/660265#M101326</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;I am working over the IMX6 solo which is interfaced with serial NOR Flash. As per the Reference Manual , Table 8-1 ,&lt;/P&gt;&lt;P&gt;Serial Downloader mode can be used for firmware flashing. But Serial Downloader mode requires serial USB. In my target board USB board is not populated. My questions are as follows :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Can I flash uboot using debug UART&amp;nbsp;? &amp;nbsp;if yes then please explain how .&lt;/P&gt;&lt;P&gt;2 . In which mode IMX6 will boot up to write the NOR Flash using UART.&lt;/P&gt;&lt;P&gt;Please suggest.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Aditya Nagal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Apr 2017 11:48:11 GMT</pubDate>
    <dc:creator>adityanagal</dc:creator>
    <dc:date>2017-04-07T11:48:11Z</dc:date>
    <item>
      <title>How uboot can be written over NOR Flash using UART</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-uboot-can-be-written-over-NOR-Flash-using-UART/m-p/660265#M101326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;I am working over the IMX6 solo which is interfaced with serial NOR Flash. As per the Reference Manual , Table 8-1 ,&lt;/P&gt;&lt;P&gt;Serial Downloader mode can be used for firmware flashing. But Serial Downloader mode requires serial USB. In my target board USB board is not populated. My questions are as follows :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Can I flash uboot using debug UART&amp;nbsp;? &amp;nbsp;if yes then please explain how .&lt;/P&gt;&lt;P&gt;2 . In which mode IMX6 will boot up to write the NOR Flash using UART.&lt;/P&gt;&lt;P&gt;Please suggest.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Aditya Nagal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Apr 2017 11:48:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-uboot-can-be-written-over-NOR-Flash-using-UART/m-p/660265#M101326</guid>
      <dc:creator>adityanagal</dc:creator>
      <dc:date>2017-04-07T11:48:11Z</dc:date>
    </item>
    <item>
      <title>Re: How uboot can be written over NOR Flash using UART</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-uboot-can-be-written-over-NOR-Flash-using-UART/m-p/660266#M101327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="282912" data-username="adityanagal" href="https://community.nxp.com/people/adityanagal"&gt;Aditya&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;1. Can I flash uboot using debug UART&amp;nbsp;? &amp;nbsp;if yes then please explain how .&lt;/P&gt;&lt;P&gt;No, you can't.&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;2 . In which mode IMX6 will boot up to write the NOR Flash using UART.&lt;/P&gt;&lt;P&gt;I.MX6 doesn't support downloading uboot by UART port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are 2 ways to write u-boot to your nor flash:&lt;/P&gt;&lt;P&gt;(1) writing u-boot to NOR Flash by USB OTG port.&lt;/P&gt;&lt;P&gt;You had better populate USB OTG connector to your board, it is very important, I don't know why not populate it.&lt;/P&gt;&lt;P&gt;(2) Using SD card to boot your system, then write u-boot image to Nor Flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope above advice can help you!&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Apr 2017 12:52:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-uboot-can-be-written-over-NOR-Flash-using-UART/m-p/660266#M101327</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2017-04-07T12:52:52Z</dc:date>
    </item>
  </channel>
</rss>