<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Write not working in framebuffer on which mipi oled connects in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Write-not-working-in-framebuffer-on-which-mipi-oled-connects/m-p/659858#M101268</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kunal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check "mxcfb*" aliases in dts file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 May 2017 10:12:00 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-05-04T10:12:00Z</dc:date>
    <item>
      <title>Write not working in framebuffer on which mipi oled connects</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Write-not-working-in-framebuffer-on-which-mipi-oled-connects/m-p/659855#M101265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While trying to interface Oled over Mipi DSI in iMX6DL board, I could see the driver code being executed because it is showing stable backlight now when it executes SLEEP_OUT command. So after it comes out of sleep, I try to write something to framebuffer.&lt;/P&gt;&lt;P&gt;But, to my surprise, I am not able to write anything to framebuffer. ie. I used this command:&lt;/P&gt;&lt;P&gt;dd if=/dev/urandom of=/dev/fb0 bs=3200 count=400&lt;/P&gt;&lt;P&gt;and was expecting some pixels to change color etc. but nothing changes. I also used a cross compiled app to write to fb0 on which mipi_dsi is supposed to have been interfaced. I am not sure whether I need to do some more changes in driver to make sure fb connects to the oled.&lt;/P&gt;&lt;P&gt;Anybody faced such kind of issues or with any clues will help me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Kunal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 May 2017 12:41:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Write-not-working-in-framebuffer-on-which-mipi-oled-connects/m-p/659855#M101265</guid>
      <dc:creator>kunalkulshresth</dc:creator>
      <dc:date>2017-05-03T12:41:37Z</dc:date>
    </item>
    <item>
      <title>Re: Write not working in framebuffer on which mipi oled connects</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Write-not-working-in-framebuffer-on-which-mipi-oled-connects/m-p/659856#M101266</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kunal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try procedure described in sect.6.5.1 Framebuffer Tests attached Linux Manual&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 May 2017 23:40:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Write-not-working-in-framebuffer-on-which-mipi-oled-connects/m-p/659856#M101266</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-05-03T23:40:05Z</dc:date>
    </item>
    <item>
      <title>Re: Write not working in framebuffer on which mipi oled connects</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Write-not-working-in-framebuffer-on-which-mipi-oled-connects/m-p/659857#M101267</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sure, I tried these tests. The problem is that nothing actually affects a change on the mipi dsi display. I assume the fb0 has been associated with the mipi_dsi driver so it could have produced an effect when I write something on fb0, but it does not.&lt;/P&gt;&lt;P&gt;I use fbset command to see the display properties (timing params) are well picked up and mipi display does show backlight when it comes out of sleep mode. Any idea how to debug fb0 association with mipi_dsi driver?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Kunal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 May 2017 05:52:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Write-not-working-in-framebuffer-on-which-mipi-oled-connects/m-p/659857#M101267</guid>
      <dc:creator>kunalkulshresth</dc:creator>
      <dc:date>2017-05-04T05:52:11Z</dc:date>
    </item>
    <item>
      <title>Re: Write not working in framebuffer on which mipi oled connects</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Write-not-working-in-framebuffer-on-which-mipi-oled-connects/m-p/659858#M101268</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kunal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check "mxcfb*" aliases in dts file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 May 2017 10:12:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Write-not-working-in-framebuffer-on-which-mipi-oled-connects/m-p/659858#M101268</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-05-04T10:12:00Z</dc:date>
    </item>
    <item>
      <title>Re: Write not working in framebuffer on which mipi oled connects</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Write-not-working-in-framebuffer-on-which-mipi-oled-connects/m-p/659859#M101269</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: #1f497d;"&gt;So, for me only enabled FBs are fb0 and fb1. And fbset gives me appropriate information for fb0 i.e. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: #1f497d;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: #1f497d;"&gt;# fbset –fb /dev/fb0&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: #1f497d;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: #1f497d;"&gt;mode “400x400-60”&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: #1f497d;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; color: #1f497d;"&gt;# D: 12.556 MHz, H: 26.158 kHz, V: 59.996 Hz&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: #1f497d;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; geometry 400 400 400 400 32&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: #1f497d;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; timings 79643 40 20 12 20 20 4&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: #1f497d;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; rgba 8/16,8/8,8/0,8/24&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: #1f497d;"&gt;endmode&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: #1f497d;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: #1f497d;"&gt;So I was of understanding that fb0 should be good to write data on. Fb2 is anyways not enabled. But I tried changing mxcfb3: fb@2 to mxcfb3:fb@0 which also did not help. Is it like it is doubtful that fb0 is enabled instead of fb2 when we see dtsi? Attached are the logs (with mxcfb3:fb@2).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: #1f497d;"&gt;Please see the logs:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: #1f497d;"&gt;Starting Xserver&lt;BR /&gt;Starting system message bus: dbus.&lt;BR /&gt;Starting Connection Manager&lt;BR /&gt;Starting Dropbear SSH server: dropbear.&lt;BR /&gt;Starting rpcbind daemon...done.&lt;BR /&gt;mxc_sdc_fb fb.23: Bfore initing panel pixclock = 12556000l Hz&lt;BR /&gt;mipi_dsi_enable_controller&lt;BR /&gt;MIPI_DSI_DPI_CFG val = 0xf4&lt;BR /&gt;mipi_dsi_enable_controller MIPI_DSI_ERROR_ST0 val = 0x0&lt;BR /&gt;mipi_dsi_enable_controller MIPI_DSI_ERROR_ST1 val = 0x0&lt;BR /&gt;initing pll config&lt;BR /&gt;In oled_reset rst_gpio 143&lt;BR /&gt;mipi_dsi 21e0000.mipi: MIPI DSI LCD setup.&lt;BR /&gt;mipi_dsi 21e0000.mipi: In mipid_hx8369_lcd_setup ...mipi_dsi-&amp;gt;mmio_base:0xf0188000.&lt;BR /&gt;MIPI_DSI_CMD_PKT_STATUS val = 0x1515&lt;BR /&gt;MIPI_DSI_CMD_PKT_STATUS val = 0x1515&lt;BR /&gt;MIPI_DSI_CMD_PKT_STATUS val = 0x1515&lt;BR /&gt;mipi_dsi 21e0000.mipi: 40 writing to 36h...OK.&lt;BR /&gt;fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:01, irq=-1)&lt;BR /&gt;IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready&lt;BR /&gt;MIPI_DSI_CMD_PKT_STATUS val = 0x1515&lt;BR /&gt;mipi_dsi_set_mode cmd_mode = 0&lt;BR /&gt;mipi_dsi_set_mode cmd_mode 0 val = 0x1ffe&lt;BR /&gt;mipi_dsi_pwr_up val = 0x1&lt;BR /&gt;Just before mipi_dsi_power_onJust before mipi_dsi_power_onmipi_dsi-&amp;gt;bl = 0&lt;BR /&gt;mipi_dsi_power_on sleepout_once = 0&lt;BR /&gt;starting statd: done&lt;BR /&gt;mxc_sdc_fb fb.23: Bfore initing panel pixclock = 12556000l Hz&lt;BR /&gt;Just before mipi_dsi_power_onmipi_dsi-&amp;gt;bl = 0&lt;BR /&gt;mipi_dsi_power_on sleepout_once = 0&lt;BR /&gt;Starting advanced power management daemon: No APM support in kernel&lt;BR /&gt;(failed.)&lt;BR /&gt;mipi_dsi_disable sleepout_once = 0&lt;BR /&gt;mipi_dsi_power_offmipi_dsi_set_mode cmd_mode = 1&lt;BR /&gt;mipi_dsi_set_mode cmd_mode 1 val = 0x1fff&lt;BR /&gt;MIPI_DSI_CMD_PKT_STATUS val = 0x1515&lt;BR /&gt;mipi_dsi_set_mode cmd_mode = 0&lt;BR /&gt;mipi_dsi_set_mode cmd_mode 0 val = 0x1ffe&lt;BR /&gt;mipi_dsi_pwr_up val = 0x1&lt;BR /&gt;mipi_dsi_set_mode cmd_mode = 1&lt;BR /&gt;mipi_dsi_set_mode cmd_mode 1 val = 0x1fff&lt;BR /&gt;mipi_dsi_disable_controllerNFS daemon support not enabled in kernel&lt;BR /&gt;&lt;BR /&gt;mxc_sdc_fb fb.23: Bfore initing panel pixclock = 12556000l Hz&lt;BR /&gt;Just before mipi_dsi_power_onmipi_dsi-&amp;gt;bl = 0&lt;BR /&gt;mipi_dsi_power_on sleepout_once = 0&lt;BR /&gt;mipi_dsi_enable_controller&lt;BR /&gt;random: nonblocking pool is initialized&lt;BR /&gt;mipi_dsi_set_mode cmd_mode = 0&lt;BR /&gt;mipi_dsi_set_mode cmd_mode 0 val = 0x1ffe&lt;BR /&gt;mipi_dsi_pwr_up val = 0x1&lt;BR /&gt;mipi_dsi_set_mode cmd_mode = 1&lt;BR /&gt;mipi_dsi_set_mode cmd_mode 1 val = 0x1fff&lt;BR /&gt;In oled_reset rst_gpio 143&lt;BR /&gt;MIPI_DSI_CMD_PKT_STATUS val = 0x1515&lt;BR /&gt;EXIT_SLEEP_MODEMIPI_DSI_CMD_PKT_STATUS val = 0x1515&lt;BR /&gt;Exit Idle Mode&lt;BR /&gt;mipi_dsi_set_mode cmd_mode = 0&lt;BR /&gt;mipi_dsi_set_mode cmd_mode 0 val = 0x1ffe&lt;BR /&gt;mipi_dsi_pwr_up val = 0x1&lt;BR /&gt;Starting syslogd/klogd: mxc_sdc_fb fb.23: Bfore initing panel pixclock = 12556000l Hz&lt;BR /&gt;Just before mipi_dsi_power_onmipi_dsi-&amp;gt;bl = 0&lt;BR /&gt;mipi_dsi_power_on sleepout_once = 1&lt;BR /&gt;done&lt;BR /&gt;mipi_dsi_disable sleepout_once = 1&lt;BR /&gt;&amp;nbsp;* Starting Avahi mDNS/DNS-SD Daemon: avahi-daemon&lt;BR /&gt;mxc_sdc_fb fb.23: Bfore initing panel pixclock = 12556000l Hz&lt;BR /&gt;Just before mipi_dsi_power_onmipi_dsi-&amp;gt;bl = 0&lt;BR /&gt;mipi_dsi_power_on sleepout_once = 1&lt;BR /&gt;[ ok ]si_disable sleepout_once = 1&lt;BR /&gt;Starting Telephony daemon&lt;BR /&gt;Starting Linux NFC daemon&lt;BR /&gt;Starting OProfileUI server&lt;BR /&gt;Starting autohdmi: &lt;BR /&gt;Running local boot scripts (/etc/rc.local).&lt;BR /&gt;&lt;BR /&gt;Poky (Yocto Project Reference Distro) 1.7 imx6dlsabreauto /dev/ttymxc3&lt;BR /&gt;&lt;BR /&gt;imx6dlsabreauto login: mxc_sdc_fb fb.23: Bfore initing panel pixclock = 12556000l Hz&lt;BR /&gt;Just before mipi_dsi_power_onmipi_dsi-&amp;gt;bl = 0&lt;BR /&gt;mipi_dsi_power_on sleepout_once = 1&lt;BR /&gt;&lt;BR /&gt;Poky (Yocto Project Reference Distro) 1.7 imx6dlsabreauto /dev/ttymxc3&lt;BR /&gt;&lt;BR /&gt;imx6dlsabreauto login: &lt;BR /&gt;Poky (Yocto Project Reference Distro) 1.7 imx6dlsabreauto /dev/ttymxc3&lt;BR /&gt;&lt;BR /&gt;imx6dlsabreauto login: &lt;BR /&gt;Poky (Yocto Project Reference Distro) 1.7 imx6dlsabreauto /dev/ttymxc3&lt;BR /&gt;&lt;BR /&gt;imx6dlsabreauto login: root&lt;BR /&gt;root@imx6dlsabreauto:~# &lt;BR /&gt;root@imx6dlsabreauto:~# &lt;BR /&gt;root@imx6dlsabreauto:~# &lt;BR /&gt;root@imx6dlsabreauto:~# cat /sys/class/graphics/fb0/&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;bits_per_pixel&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl_disp_property&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; state&lt;BR /&gt;blank&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mode&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; stride&lt;BR /&gt;console&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; modes&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; subsystem/&lt;BR /&gt;cursor&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; name&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uevent&lt;BR /&gt;dev&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pan&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; virtual_size&lt;BR /&gt;device/&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; power/&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;fsl_disp_dev_property&amp;nbsp; rotate&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;root@imx6dlsabreauto:~# cat /sys/class/graphics/fb0/fsl_disp_dev_property &lt;BR /&gt;mipi_dsi&lt;BR /&gt;root@imx6dlsabreauto:~# &lt;BR /&gt;root@imx6dlsabreauto:~# &lt;BR /&gt;root@imx6dlsabreauto:~# fbset -fb /dev/fb0&lt;BR /&gt;&lt;BR /&gt;mode "400x400-60"&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; # D: 12.556 MHz, H: 26.158 kHz, V: 59.996 Hz&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; geometry 400 400 400 400 32&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; timings 79643 40 20 12 20 20 4&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; rgba 8/16,8/8,8/0,8/24&lt;BR /&gt;endmode&lt;BR /&gt;&lt;BR /&gt;root@imx6dlsabreauto:~# &lt;BR /&gt;root@imx6dlsabreauto:~# ls&lt;BR /&gt;FirstDisp&amp;nbsp;&amp;nbsp; WriteToFB&amp;nbsp; images.jpeg&amp;nbsp; pic1.jpg&amp;nbsp; pic2.jpg&lt;BR /&gt;QtQuickApp&amp;nbsp; data&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pic1.c&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pic2.c&amp;nbsp;&amp;nbsp;&amp;nbsp; s&lt;BR /&gt;root@imx6dlsabreauto:~# cat /dev/urandom &amp;gt; /dev/fb0 &lt;BR /&gt;fb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_write^V^C&lt;BR /&gt;root@imx6dlsabreauto:~# dd if=/dev/urandom of=/dev/fb0 bs=3200 count=400&lt;BR /&gt;fb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_writefb_wn&lt;BR /&gt;400+0 records out&lt;BR /&gt;1280000 bytes (1.3 MB) copied, 0.915004 s, 1.4 MB/s&lt;BR /&gt;root@imx6dlsabreauto:~# ^M&lt;BR /&gt;-sh: $'\r': command not found&lt;BR /&gt;root@imx6dlsabreauto:~# &lt;BR /&gt;root@imx6dlsabreauto:~# &lt;BR /&gt;root@imx6dlsabreauto:~# &lt;BR /&gt;root@imx6dlsabreauto:~# &lt;BR /&gt;root@imx6dlsabreauto:~# &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .text : 0x80008000 - 0x80d1261c&amp;nbsp;&amp;nbsp; (13354 kB)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: #1f497d;"&gt;Thanks and regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: #1f497d;"&gt;Kunal&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 May 2017 05:30:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Write-not-working-in-framebuffer-on-which-mipi-oled-connects/m-p/659859#M101269</guid>
      <dc:creator>kunalkulshresth</dc:creator>
      <dc:date>2017-05-05T05:30:30Z</dc:date>
    </item>
  </channel>
</rss>