<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to output 25 MHz Clock from RGMII_TXC pin in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-output-25-MHz-Clock-from-RGMII-TXC-pin/m-p/659328#M101167</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mehmet,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My apologies for not being clear. I believe your scenario is similar to the one described on the following thread:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/360116"&gt;https://community.nxp.com/message/539982&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you wish to generate the PHY clock on the i.MX6 you may do so but you should use either GPIO_16 or RGMII_TX_CTL as output; and then input the 125MHZ from the PHY to ENET_REF_CLK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The reason being that the RGMII_TXC pin is generated from the ENET module but the module itself requires the 125Mhz clock for RGMII. RGMII_TXC should thus be used as signal for the RGMII but not as reference clock.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pins GPIO_16 or RGMII_TX_CTL may be used to generate the clock from the PLLs and then provide to the PHY. These pins would be controlled with register CCM_ANALOG_PLL_ENETn.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Mar 2017 20:21:09 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2017-03-17T20:21:09Z</dc:date>
    <item>
      <title>How to output 25 MHz Clock from RGMII_TXC pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-output-25-MHz-Clock-from-RGMII-TXC-pin/m-p/659325#M101164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have i.mx6dl based board with Micrel KSZ9021 PHY. &amp;nbsp;PHY needs 25 MHz clock from MX6 MAC to generate 125 MHz reference clock, in its RGMII mode.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using u-boot 2009.08. &amp;nbsp;There is 6 MHz clock at RGMII_TXC pin. Is it possible to output 25 MHz clock from this pin? &amp;nbsp;If yes, How can I do it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and best regards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mehmet Ali Ipin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Mar 2017 12:47:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-output-25-MHz-Clock-from-RGMII-TXC-pin/m-p/659325#M101164</guid>
      <dc:creator>mehmetipin</dc:creator>
      <dc:date>2017-03-16T12:47:34Z</dc:date>
    </item>
    <item>
      <title>Re: How to output 25 MHz Clock from RGMII_TXC pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-output-25-MHz-Clock-from-RGMII-TXC-pin/m-p/659326#M101165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mehmet Ali Ipin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can find information on how to achieve this in section 10.4.2 of the i.MX6 Hardware Guide (link below).&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/assets/documents/data/en/user-guides/IMX6DQ6SDLHDG.pdf"&gt;http://www.nxp.com/assets/documents/data/en/user-guides/IMX6DQ6SDLHDG.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please also look at bits CCM_ANALOG_PLL_ENETn[0:1], as listed on section 18.7.15 of the i.MX6Q Reference Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information helps!&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Mar 2017 21:52:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-output-25-MHz-Clock-from-RGMII-TXC-pin/m-p/659326#M101165</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2017-03-16T21:52:27Z</dc:date>
    </item>
    <item>
      <title>Re: How to output 25 MHz Clock from RGMII_TXC pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-output-25-MHz-Clock-from-RGMII-TXC-pin/m-p/659327#M101166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Gusarambula,&lt;/P&gt;&lt;P&gt;Thank you very much for your informations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I read section 10.4.2 of Hardware guide. It explains RGMII_TX_CTL pin to generate the reference clock, and there is nothing with RGMII_TXC pin. &amp;nbsp;I am very confused;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Are we using RGMII_TX_CTL pin&amp;nbsp;in order to output clock signal from RGMII_TXC pin?&lt;/LI&gt;&lt;LI&gt;Is it possible to generate 25 MHz clock at the&amp;nbsp;RGMII_TXC pin?&lt;/LI&gt;&lt;LI&gt;What is the reference of RGMII_TXC&amp;nbsp;clock CCM_ANALOG_PLL_ENETn&amp;nbsp; or external 125 MHz?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mehmet&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Mar 2017 07:19:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-output-25-MHz-Clock-from-RGMII-TXC-pin/m-p/659327#M101166</guid>
      <dc:creator>MehmetAliIpin</dc:creator>
      <dc:date>2017-03-17T07:19:24Z</dc:date>
    </item>
    <item>
      <title>Re: How to output 25 MHz Clock from RGMII_TXC pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-output-25-MHz-Clock-from-RGMII-TXC-pin/m-p/659328#M101167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mehmet,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My apologies for not being clear. I believe your scenario is similar to the one described on the following thread:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/360116"&gt;https://community.nxp.com/message/539982&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you wish to generate the PHY clock on the i.MX6 you may do so but you should use either GPIO_16 or RGMII_TX_CTL as output; and then input the 125MHZ from the PHY to ENET_REF_CLK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The reason being that the RGMII_TXC pin is generated from the ENET module but the module itself requires the 125Mhz clock for RGMII. RGMII_TXC should thus be used as signal for the RGMII but not as reference clock.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pins GPIO_16 or RGMII_TX_CTL may be used to generate the clock from the PLLs and then provide to the PHY. These pins would be controlled with register CCM_ANALOG_PLL_ENETn.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Mar 2017 20:21:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-output-25-MHz-Clock-from-RGMII-TXC-pin/m-p/659328#M101167</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2017-03-17T20:21:09Z</dc:date>
    </item>
    <item>
      <title>Re: How to output 25 MHz Clock from RGMII_TXC pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-output-25-MHz-Clock-from-RGMII-TXC-pin/m-p/659329#M101168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Gusarambula,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your pations and informations; Unfortunately&amp;nbsp;I don't have GPIO_16 pin to generate 125MHz clock. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know MAC needs 125 MHZ clock from PHY/or external source. PHY(9021) also needs 25 MHz clock in its GTX_CLK pin&amp;nbsp;to generate 125 MHz ENET_REF_CLK. My PHY&amp;nbsp;schematic is same as MCIMX6QP-SDB. I connected RGMII_TXC to GTX_CLK and RGMII_TX_CTL pin TX_EN&amp;nbsp;pin of PHY.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In fact&amp;nbsp;I Have 6 MHz at RGMII_TXC pin, and PHY is generating 30 MHz(5*GTX_CLK) (if it was 25, PHY will generate 125MHz) to ENET_REF_CLK pin of MX6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I only need informations, what should I do to generate 25 MHz clock instead of 6 MHz from RGMII_TXC pin?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Mar 2017 07:32:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-output-25-MHz-Clock-from-RGMII-TXC-pin/m-p/659329#M101168</guid>
      <dc:creator>mehmetipin</dc:creator>
      <dc:date>2017-03-20T07:32:33Z</dc:date>
    </item>
    <item>
      <title>Re: How to output 25 MHz Clock from RGMII_TXC pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-output-25-MHz-Clock-from-RGMII-TXC-pin/m-p/659330#M101169</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mehmet Ali Ipin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm currently double checking if it's possible to generate the 25Mhz clock from RGMII_TXC as your design requires. I'll update this thread as soon as I have more information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Mar 2017 23:24:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-output-25-MHz-Clock-from-RGMII-TXC-pin/m-p/659330#M101169</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2017-03-24T23:24:53Z</dc:date>
    </item>
    <item>
      <title>Re: How to output 25 MHz Clock from RGMII_TXC pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-output-25-MHz-Clock-from-RGMII-TXC-pin/m-p/659331#M101170</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Gusarambula,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your interests.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 Mar 2017 16:55:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-output-25-MHz-Clock-from-RGMII-TXC-pin/m-p/659331#M101170</guid>
      <dc:creator>MehmetAliIpin</dc:creator>
      <dc:date>2017-03-25T16:55:40Z</dc:date>
    </item>
    <item>
      <title>Re: How to output 25 MHz Clock from RGMII_TXC pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-output-25-MHz-Clock-from-RGMII-TXC-pin/m-p/659332#M101171</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mehmet Ali Ipin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My apologies. I double checked and confirmed that it’s not possible to multiplex RGMII_TXC as 25MHz reference clock output for RGMII PHY.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX6Q can output a 50MHz reference clock from GPIO_16 or RGMII_TX_CTL for RMII application. If GPIO_16 is available, it might be able to output a 25MHz clock for the RGMII PHY.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In your case since GPIO_16 is not available the best alternative would be adding a 25MHz crystal on the PHY since the RGMII_TXC pin cannot generate it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Mar 2017 17:07:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-output-25-MHz-Clock-from-RGMII-TXC-pin/m-p/659332#M101171</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2017-03-28T17:07:47Z</dc:date>
    </item>
    <item>
      <title>Re: How to output 25 MHz Clock from RGMII_TXC pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-output-25-MHz-Clock-from-RGMII-TXC-pin/m-p/659333#M101172</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Gusarambula,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your informations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Mar 2017 06:00:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-output-25-MHz-Clock-from-RGMII-TXC-pin/m-p/659333#M101172</guid>
      <dc:creator>MehmetAliIpin</dc:creator>
      <dc:date>2017-03-30T06:00:06Z</dc:date>
    </item>
  </channel>
</rss>