<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Difference between packaging in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-packaging/m-p/659236#M101151</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please note that these package differs a bit with pin configuration.&lt;BR /&gt;For example 12x12 one has no pins related to ADC2. &lt;BR /&gt;Please refer pitch ball map you can find in the Datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 May 2017 02:00:33 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2017-05-04T02:00:33Z</dc:date>
    <item>
      <title>Difference between packaging</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-packaging/m-p/659235#M101150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;BR /&gt;This question may sound silly, but I would like to have more information about the i.MX7 packages difference.&lt;BR /&gt;What is the advantage of the 19 * 19mm version given that the 12 * 12 is cheaper?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards, Johyn Papin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 May 2017 17:22:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Difference-between-packaging/m-p/659235#M101150</guid>
      <dc:creator>johynpapin</dc:creator>
      <dc:date>2017-05-02T17:22:29Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between packaging</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-packaging/m-p/659236#M101151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please note that these package differs a bit with pin configuration.&lt;BR /&gt;For example 12x12 one has no pins related to ADC2. &lt;BR /&gt;Please refer pitch ball map you can find in the Datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 May 2017 02:00:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Difference-between-packaging/m-p/659236#M101151</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2017-05-04T02:00:33Z</dc:date>
    </item>
  </channel>
</rss>