<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX535 processor interfacing with 8 bit Parallel Camera- HSYNC and MCLK pins</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX535-processor-interfacing-with-8-bit-Parallel-Camera-HSYNC/m-p/659136#M101122</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, We are planning to use&amp;nbsp;MCIMX535DVV1C for one of medical device. In our Application we need to interface a 8 bit camera to iMX processor after going through the datasheet, Reference Manual and User guide we are confused about pin Number of HSYNC and MCLK pins that we need to interface to our Camera chip. Page number 200 of&amp;nbsp;MX53UG Rev. 2 06/2015 illustrates HSYNC and MCLK signal shall be a separate pin but datasheet of iMX53 does not depict pin for HSYNC. Kindly guide us on this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Mar 2017 13:19:19 GMT</pubDate>
    <dc:creator>jhalife</dc:creator>
    <dc:date>2017-03-16T13:19:19Z</dc:date>
    <item>
      <title>iMX535 processor interfacing with 8 bit Parallel Camera- HSYNC and MCLK pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX535-processor-interfacing-with-8-bit-Parallel-Camera-HSYNC/m-p/659136#M101122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, We are planning to use&amp;nbsp;MCIMX535DVV1C for one of medical device. In our Application we need to interface a 8 bit camera to iMX processor after going through the datasheet, Reference Manual and User guide we are confused about pin Number of HSYNC and MCLK pins that we need to interface to our Camera chip. Page number 200 of&amp;nbsp;MX53UG Rev. 2 06/2015 illustrates HSYNC and MCLK signal shall be a separate pin but datasheet of iMX53 does not depict pin for HSYNC. Kindly guide us on this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Mar 2017 13:19:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX535-processor-interfacing-with-8-bit-Parallel-Camera-HSYNC/m-p/659136#M101122</guid>
      <dc:creator>jhalife</dc:creator>
      <dc:date>2017-03-16T13:19:19Z</dc:date>
    </item>
    <item>
      <title>Re: iMX535 processor interfacing with 8 bit Parallel Camera- HSYNC and MCLK pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX535-processor-interfacing-with-8-bit-Parallel-Camera-HSYNC/m-p/659137#M101123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Gopal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you already suffer, there is a some options available for this pins, in order to select the proper, you can use the IOMUX tool, this would help you to identify, configure and generate the necessary to use one of the options for the CSI port or any of the peripherals of the device.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jaime&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Mar 2017 18:27:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX535-processor-interfacing-with-8-bit-Parallel-Camera-HSYNC/m-p/659137#M101123</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2017-03-28T18:27:11Z</dc:date>
    </item>
    <item>
      <title>Re: iMX535 processor interfacing with 8 bit Parallel Camera- HSYNC and MCLK pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX535-processor-interfacing-with-8-bit-Parallel-Camera-HSYNC/m-p/659138#M101124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Mar 2017 02:40:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX535-processor-interfacing-with-8-bit-Parallel-Camera-HSYNC/m-p/659138#M101124</guid>
      <dc:creator>jhalife</dc:creator>
      <dc:date>2017-03-29T02:40:38Z</dc:date>
    </item>
  </channel>
</rss>