<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Which is valid if both DISABLE_PSWITCH bit and AUTO_RESTART bit enabled.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Which-is-valid-if-both-DISABLE-PSWITCH-bit-and-AUTO-RESTART-bit/m-p/658913#M101092</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your quick response.&lt;/P&gt;&lt;P&gt;I read 11.3 of Reference Manual and have 3 question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1)&amp;nbsp;How to defined VDDXTAL voltage?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;Who generate VDDXTAL pin output?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2)&amp;nbsp;HW_RTC_PERSISTENT0_AUTO_RESTART bit can be controlled to on/off&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; the internal 5-KΩ register between PSWITCH and VDDXTAL?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; If AUTO_RESTART bit is enabled, PSWITCH connected to VDDXTAL by internal register.&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; As a result, voltage level would be PSWITCH = VDDXTAL and will be detected MID level.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Is it correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3)&amp;nbsp;MID level of PSWITCH seems less than VDDXTAL, So DISABLE_PSWITCH bit should effect&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; only recovery mode function compared with HIGH LEVEL voltage?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ishii.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Dec 2016 10:04:00 GMT</pubDate>
    <dc:creator>t-iishii</dc:creator>
    <dc:date>2016-12-14T10:04:00Z</dc:date>
    <item>
      <title>Which is valid if both DISABLE_PSWITCH bit and AUTO_RESTART bit enabled.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-is-valid-if-both-DISABLE-PSWITCH-bit-and-AUTO-RESTART-bit/m-p/658908#M101087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In i.MX28, if DISABLE_PSWITH bit and AUTO_RESTART bit are enabled,&lt;/P&gt;&lt;P&gt;Which function will work?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; 1)&amp;nbsp;Disables the pswitch pin startup functionality unless the voltage on the pswitch pin goes above the&lt;BR /&gt;VDDXTAL pin voltage by a threshold voltage.&lt;/P&gt;&lt;P&gt;&amp;nbsp; 2)&amp;nbsp;Set to one to enable the chip to automatically power up approximately 180 ms after powering down.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ishii.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Dec 2016 10:26:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-is-valid-if-both-DISABLE-PSWITCH-bit-and-AUTO-RESTART-bit/m-p/658908#M101087</guid>
      <dc:creator>t-iishii</dc:creator>
      <dc:date>2016-12-08T10:26:11Z</dc:date>
    </item>
    <item>
      <title>Re: Which is valid if both DISABLE_PSWITCH bit and AUTO_RESTART bit enabled.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-is-valid-if-both-DISABLE-PSWITCH-bit-and-AUTO-RESTART-bit/m-p/658909#M101088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ishii&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems DISABLE_PSWITH takes priority, as AUTO_RESTART just&lt;/P&gt;&lt;P&gt;gives another way to use DISABLE_PSWITH functionality.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Dec 2016 23:34:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-is-valid-if-both-DISABLE-PSWITCH-bit-and-AUTO-RESTART-bit/m-p/658909#M101088</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-12-08T23:34:02Z</dc:date>
    </item>
    <item>
      <title>Re: Which is valid if both DISABLE_PSWITCH bit and AUTO_RESTART bit enabled.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-is-valid-if-both-DISABLE-PSWITCH-bit-and-AUTO-RESTART-bit/m-p/658910#M101089</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear igor&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand that DISABLE_PSWITCH setting is strong than AUTO_RESTART setting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ishii&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 01:29:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-is-valid-if-both-DISABLE-PSWITCH-bit-and-AUTO-RESTART-bit/m-p/658910#M101089</guid>
      <dc:creator>t-iishii</dc:creator>
      <dc:date>2016-12-09T01:29:45Z</dc:date>
    </item>
    <item>
      <title>Re: Which is valid if both DISABLE_PSWITCH bit and AUTO_RESTART bit enabled.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-is-valid-if-both-DISABLE-PSWITCH-bit-and-AUTO-RESTART-bit/m-p/658911#M101090</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our customer says that their board will boot up though both condition are enable.&lt;/P&gt;&lt;P&gt;It seems that DISABLE_PSWITCH enable enable is not functioning.&lt;/P&gt;&lt;P&gt;&amp;nbsp;1) DISABLE_PSWITCH = 1 and AUTO_RESTART = 1&lt;/P&gt;&lt;P&gt;&amp;nbsp;2) PSWITCH pin voltage &amp;lt; VDDXTAL pin voltage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you know another condition to power up the device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our customer design to use DCDC_BATT source only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ishii.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Dec 2016 09:30:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-is-valid-if-both-DISABLE-PSWITCH-bit-and-AUTO-RESTART-bit/m-p/658911#M101090</guid>
      <dc:creator>t-iishii</dc:creator>
      <dc:date>2016-12-12T09:30:23Z</dc:date>
    </item>
    <item>
      <title>Re: Which is valid if both DISABLE_PSWITCH bit and AUTO_RESTART bit enabled.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-is-valid-if-both-DISABLE-PSWITCH-bit-and-AUTO-RESTART-bit/m-p/658912#M101091</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ishii&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;how customer starts-up board with DCDC_BATT source only design&lt;/P&gt;&lt;P&gt;and disabled PSWITCH .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Do you know another condition to power up the device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check sect.11.3.3 Power-Up Sequence i.MX28 Reference Manual&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2Fdsp%2Fdoc%2Fref_manual%2FMCIMX28RM.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/dsp/doc/ref_manual/MCIMX28RM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Dec 2016 10:05:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-is-valid-if-both-DISABLE-PSWITCH-bit-and-AUTO-RESTART-bit/m-p/658912#M101091</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-12-12T10:05:14Z</dc:date>
    </item>
    <item>
      <title>Re: Which is valid if both DISABLE_PSWITCH bit and AUTO_RESTART bit enabled.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-is-valid-if-both-DISABLE-PSWITCH-bit-and-AUTO-RESTART-bit/m-p/658913#M101092</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your quick response.&lt;/P&gt;&lt;P&gt;I read 11.3 of Reference Manual and have 3 question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1)&amp;nbsp;How to defined VDDXTAL voltage?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;Who generate VDDXTAL pin output?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2)&amp;nbsp;HW_RTC_PERSISTENT0_AUTO_RESTART bit can be controlled to on/off&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; the internal 5-KΩ register between PSWITCH and VDDXTAL?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; If AUTO_RESTART bit is enabled, PSWITCH connected to VDDXTAL by internal register.&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; As a result, voltage level would be PSWITCH = VDDXTAL and will be detected MID level.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Is it correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3)&amp;nbsp;MID level of PSWITCH seems less than VDDXTAL, So DISABLE_PSWITCH bit should effect&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; only recovery mode function compared with HIGH LEVEL voltage?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ishii.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 10:04:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-is-valid-if-both-DISABLE-PSWITCH-bit-and-AUTO-RESTART-bit/m-p/658913#M101092</guid>
      <dc:creator>t-iishii</dc:creator>
      <dc:date>2016-12-14T10:04:00Z</dc:date>
    </item>
    <item>
      <title>Re: Which is valid if both DISABLE_PSWITCH bit and AUTO_RESTART bit enabled.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-is-valid-if-both-DISABLE-PSWITCH-bit-and-AUTO-RESTART-bit/m-p/658914#M101093</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ishii&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&amp;nbsp; VDDXTAL is generated internally when processor powered through Battery or +5V.&lt;BR /&gt;2.correct&lt;BR /&gt;3. from Table 11-1. PSWITCH Input Characteristics i.MX28 RM :&lt;BR /&gt;"A MID LEVEL PSWITCH state can be generated by connecting the VDDXTAL &lt;BR /&gt;output of the SOC to PSWITCH through a switch."&lt;BR /&gt;Customer can check DISABLE_PSWITCH = 1 by applying external voltage to &lt;BR /&gt;PSWITCH pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 23:47:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-is-valid-if-both-DISABLE-PSWITCH-bit-and-AUTO-RESTART-bit/m-p/658914#M101093</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-12-14T23:47:12Z</dc:date>
    </item>
    <item>
      <title>Re: Which is valid if both DISABLE_PSWITCH bit and AUTO_RESTART bit enabled.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-is-valid-if-both-DISABLE-PSWITCH-bit-and-AUTO-RESTART-bit/m-p/658915#M101094</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello igor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your quick response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand to use DISABLE_PSWITCH function to control restart function by applying external voltage,&lt;/P&gt;&lt;P&gt;AUTO_RESTART bit must set to be disabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ishii.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 01:19:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-is-valid-if-both-DISABLE-PSWITCH-bit-and-AUTO-RESTART-bit/m-p/658915#M101094</guid>
      <dc:creator>t-iishii</dc:creator>
      <dc:date>2016-12-15T01:19:32Z</dc:date>
    </item>
  </channel>
</rss>