<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX6DQ register settings.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-register-settings/m-p/658841#M101081</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;A1. The bits 12-8 0f the PMU_REG_1P1 register define the target output voltage of the LDO_1P1 regulator. It is recommended to keep unchanged their default value of 0x10 (meaning the target output voltage of 1.1V) as well as the default value of the bits 6-4 that define the target brownout value 175mV lower than the target output voltage (0.925V for the case under consideration).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The bits 3-0 of the PMU_REG_1P1 register should also be kept at their default values. Enabling the pulldown on the regulator's output by setting the ENABLE_PULLDOWN bit allows faster discharge of the 1P1 power rail during the system power off.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A2. The bits 12-8 of the PMU_REG_3P0 register define the target output voltage of the LDO_3P0 regulator. It is recommended to keep unchanged their default value of 0x0F (meaning the target output voltage of 3.0V) as well as the default value of the bits 6-4 that define the target brownout value 175mV lower than the target output voltage (2.825V for the case under consideration).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The bits 2-0 of the PMU_REG_3P0 register should be kept at their default values.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If USB is not used at all, the value of the bit 7 (VBUS_SEL) of the PMU_REG_3P0 register has no matter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A3. The bits 12-8 0f the PMU_REG_2P5 register define the target output voltage of the LDO_2P5 regulator. It is recommended to keep unchanged their default value of 0x10 (meaning the target output voltage of 2.5V) as well as the default value of the bits 6-4 that define the target brownout value 175mV lower than the target output voltage (2.325V for the case under consideration).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The bits 18 and 3-0 of the PMU_REG_2P5 register should be kept at their default values.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Enabling the pulldown on the regulator's output by setting the ENABLE_PULLDOWN bit allows faster discharge of the 2P5 power rail during the system power off.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A4.&lt;/P&gt;&lt;P&gt;&amp;gt; Is it possible to limit the current at LDO_ARM, LDO_SOC, LDO_PU startup time?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; How do I set the appropriate voltage for each voltage?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For target output voltage settings, please refer to the "Operating Ranges" table of the processor's Data Sheet document.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A5.&lt;/P&gt;&lt;P&gt;&amp;gt; Is it OK if STOP_MODE_CONFIG is set to "1" only, otherwise set to "0"?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It depends on what kind of STOP mode, Deep or Ligh, do you want to put the processor to.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A6.&lt;/P&gt;&lt;P&gt;&amp;gt; There was no description about w1c of bi-31-29 Hou do I set ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These status bits are set by hardware when the corresponding interrupt condition raises. Write '1' to clear each of these bits, if set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; The setting value of bit 13 - 10 is not described. How do I set it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These bits are not related to PMU. They are used to configure the external CLK1_P/N and CLK2_P/N differential clocks as inputs or outputs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; Bit 9 - 0 relates to CCM, but here is how Should I set it? Is it necessary to match with the CCM register value?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually, the PMU_MISC1n register is just the mirrored copy of the CCM_ANALOG_MISC1n register of CCM. So, you can program the CCM_ANALOG_MISC1n register and view the changes in the PMU_MISC1n one and vice versa.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A7.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; Is Brownout target of bi18 - 16, bit 1 - 0 - 8, bit 2 - 0 correct in ReadOnly? If setting is necessary, the proper value is not understood. How do I set it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Of course, these bits are r/w, not read-only, this is just a typo in the manual. It's better to keep the maximum brownout offset, i.e. set these bits to 0b111.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; For ## _ ENABLE _ ##, bit setting value is not described. How do I set it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You should set these ##_ENABLE_## bits to 1 to enable the brownout detection feature on the corresponding core domain regulator.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; Do I have to match CCM settings on the bit 31-30 of VIDEO_DIV, bit 23 of &lt;BR /&gt;AUDIO_DIV_MSB, bit 15 of AUDIO_DIV_LSB,bit 7 of PLL3_disable ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The CCM_ANALOG_MISC2n register in CCM is just the mirrored copy of the PMU_MISC2n of PMU. So, all changes are reflected automatically.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; I do not know the best value of REG # _ STEP_TIME. How do I set it&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Better to keep them at their default values of 0b00.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Mar 2017 11:45:09 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2017-03-02T11:45:09Z</dc:date>
    <item>
      <title>i.MX6DQ register settings.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-register-settings/m-p/658840#M101080</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear community.&lt;/P&gt;&lt;P&gt;Our customer has question below.&amp;nbsp;I am sorry that there are so many.&lt;SPAN style="display: none;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Question1&lt;/P&gt;&lt;P&gt;About &amp;nbsp;50.7.1 Regulator 1P1 Register (PMU_REG_1P1) of i.MX6DQRM.&lt;/P&gt;&lt;P&gt;1-1 The proper value of Brownout target of bi12 - 8 is not known.&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; In the case how do I set it?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1-2 &amp;nbsp;The setting value of bit 3 - 0 is not described.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; How do I set it?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Also, what affects setting pull down?&lt;/SPAN&gt;&lt;SPAN style="display: none;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Question2&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;About 50.7.2 Regulator 3P0 Register (PMU_REG_3P0) of i.MX6DQRM.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2-1 &lt;SPAN lang="en"&gt;· The proper value of Brownout target of bi12 - 8 is not known.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; How do I set it?&lt;BR /&gt;2-2&amp;nbsp; &amp;nbsp;The setting value of bit 2 - 0 is not described.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; How do I set it?&lt;BR /&gt;2-3&amp;nbsp; &amp;nbsp;When not using USB, how can I set VBUS_SEL?&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Should it be OnTheGo rather than a host?&lt;/SPAN&gt;&lt;SPAN style="display: none;"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;Question 3&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;About&amp;nbsp; 50.7.3 Regulator 2P5 Register (PMU_REG_2P5) of i.MX6DQRM.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;3-1&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;The proper value of Brownout target of bi12 - 8 is not known.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; How do I set it?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3-2&amp;nbsp; There is no description of the setting value of bit 18, bit 3 - 0.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; How do I set it?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Also, what affects setting pull down?&lt;/SPAN&gt;&lt;SPAN style="display: none;"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;Question 4&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;About 50.7.4 Digital Regulator Core Register (PMU_REG_CORE)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;4-1 &amp;nbsp;Is it possible to limit the current at LDO_ARM, LDO_SOC, LDO_PU startup time?&lt;BR /&gt;&lt;SPAN&gt;4-2&amp;nbsp; &amp;nbsp;How do I set the appropriate voltage for each voltage?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ARM is 792 MHz = min 1.15 V&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; VPU is 264 MHz = min 1.15 V&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (VDD_ARM_CAP) - (VDD SOC) &amp;lt;100 mV&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (VDD_ARM_CAP) - (PU_CAP) &amp;lt;100 mV&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.150 - 1.225 = - 0.075 = - 75 mV &amp;lt;100 mV: OK&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;&lt;SPAN&gt;Question 5&amp;nbsp; 50.7.5 Miscellaneous Register 0 (PMU_MISC0)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;&lt;SPAN&gt;5-1&amp;nbsp; Is it OK if STOP_MODE_CONFIG is set to "1" only, otherwise set to "0"?&lt;SPAN style="display: none;"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;&lt;SPAN&gt;Question 6&amp;nbsp; 50.7.6 Miscellaneous Register 1 (PMU_MISC1n)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;&lt;SPAN&gt;6-1 There was no description about w1c of bi-31-29&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Hou do I set ?&lt;BR /&gt;6-2&amp;nbsp; The setting value of bit 13 - 10 is not described.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; How do I set it?&lt;BR /&gt;6-3&amp;nbsp; &amp;nbsp;Bit 9 - 0 relates to CCM, but here is how Should I set it?&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Is it necessary to match with the CCM register value?&lt;SPAN style="display: none;"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;&lt;SPAN&gt;Question 7 50.7.7 Miscellaneous Control Register (PMU_MISC2n)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;&lt;SPAN&gt;7-1&amp;nbsp; Is Brownout target of bi18 - 16, bit 1 - 0 - 8, bit 2 - 0 correct in ReadOnly?&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; If setting is necessary, the proper value is not understood. How do I set it?&lt;BR /&gt;7-2&amp;nbsp; For ## _ ENABLE _ ##, bit setting value is not described.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; How do I set it?&lt;BR /&gt;7-3&amp;nbsp; Do I have to match CCM settings on the&amp;nbsp; bit 31-30 of VIDEO_DIV, bit 23 of AUDIO_DIV_MSB, bit 15 of&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; AUDIO_DIV_LSB,bit 7 of PLL3_disable&amp;nbsp;&amp;nbsp;?&lt;BR /&gt;&amp;nbsp;7-4&amp;nbsp; I do not know the best value of REG # _ STEP_TIME. How do I set it&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;&lt;SPAN&gt;Thank you,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;&lt;SPAN&gt;Best Regards.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;&lt;SPAN&gt;Takashi&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 06:18:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-register-settings/m-p/658840#M101080</guid>
      <dc:creator>takashitakahash</dc:creator>
      <dc:date>2017-02-22T06:18:19Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6DQ register settings.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-register-settings/m-p/658841#M101081</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;A1. The bits 12-8 0f the PMU_REG_1P1 register define the target output voltage of the LDO_1P1 regulator. It is recommended to keep unchanged their default value of 0x10 (meaning the target output voltage of 1.1V) as well as the default value of the bits 6-4 that define the target brownout value 175mV lower than the target output voltage (0.925V for the case under consideration).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The bits 3-0 of the PMU_REG_1P1 register should also be kept at their default values. Enabling the pulldown on the regulator's output by setting the ENABLE_PULLDOWN bit allows faster discharge of the 1P1 power rail during the system power off.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A2. The bits 12-8 of the PMU_REG_3P0 register define the target output voltage of the LDO_3P0 regulator. It is recommended to keep unchanged their default value of 0x0F (meaning the target output voltage of 3.0V) as well as the default value of the bits 6-4 that define the target brownout value 175mV lower than the target output voltage (2.825V for the case under consideration).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The bits 2-0 of the PMU_REG_3P0 register should be kept at their default values.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If USB is not used at all, the value of the bit 7 (VBUS_SEL) of the PMU_REG_3P0 register has no matter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A3. The bits 12-8 0f the PMU_REG_2P5 register define the target output voltage of the LDO_2P5 regulator. It is recommended to keep unchanged their default value of 0x10 (meaning the target output voltage of 2.5V) as well as the default value of the bits 6-4 that define the target brownout value 175mV lower than the target output voltage (2.325V for the case under consideration).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The bits 18 and 3-0 of the PMU_REG_2P5 register should be kept at their default values.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Enabling the pulldown on the regulator's output by setting the ENABLE_PULLDOWN bit allows faster discharge of the 2P5 power rail during the system power off.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A4.&lt;/P&gt;&lt;P&gt;&amp;gt; Is it possible to limit the current at LDO_ARM, LDO_SOC, LDO_PU startup time?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; How do I set the appropriate voltage for each voltage?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For target output voltage settings, please refer to the "Operating Ranges" table of the processor's Data Sheet document.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A5.&lt;/P&gt;&lt;P&gt;&amp;gt; Is it OK if STOP_MODE_CONFIG is set to "1" only, otherwise set to "0"?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It depends on what kind of STOP mode, Deep or Ligh, do you want to put the processor to.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A6.&lt;/P&gt;&lt;P&gt;&amp;gt; There was no description about w1c of bi-31-29 Hou do I set ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These status bits are set by hardware when the corresponding interrupt condition raises. Write '1' to clear each of these bits, if set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; The setting value of bit 13 - 10 is not described. How do I set it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These bits are not related to PMU. They are used to configure the external CLK1_P/N and CLK2_P/N differential clocks as inputs or outputs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; Bit 9 - 0 relates to CCM, but here is how Should I set it? Is it necessary to match with the CCM register value?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually, the PMU_MISC1n register is just the mirrored copy of the CCM_ANALOG_MISC1n register of CCM. So, you can program the CCM_ANALOG_MISC1n register and view the changes in the PMU_MISC1n one and vice versa.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A7.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; Is Brownout target of bi18 - 16, bit 1 - 0 - 8, bit 2 - 0 correct in ReadOnly? If setting is necessary, the proper value is not understood. How do I set it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Of course, these bits are r/w, not read-only, this is just a typo in the manual. It's better to keep the maximum brownout offset, i.e. set these bits to 0b111.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; For ## _ ENABLE _ ##, bit setting value is not described. How do I set it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You should set these ##_ENABLE_## bits to 1 to enable the brownout detection feature on the corresponding core domain regulator.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; Do I have to match CCM settings on the bit 31-30 of VIDEO_DIV, bit 23 of &lt;BR /&gt;AUDIO_DIV_MSB, bit 15 of AUDIO_DIV_LSB,bit 7 of PLL3_disable ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The CCM_ANALOG_MISC2n register in CCM is just the mirrored copy of the PMU_MISC2n of PMU. So, all changes are reflected automatically.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; I do not know the best value of REG # _ STEP_TIME. How do I set it&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Better to keep them at their default values of 0b00.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Mar 2017 11:45:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DQ-register-settings/m-p/658841#M101081</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2017-03-02T11:45:09Z</dc:date>
    </item>
  </channel>
</rss>