<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How to build Native ARM compiler</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-build-Native-ARM-compiler/m-p/658723#M101071</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raana,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First add the following packet in your &amp;lt;build_dir&amp;gt;/conf/local.conf file&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IMAGE_INSTALL_append += "\&lt;/P&gt;&lt;P&gt;packagegroup-sdk-target \&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The build (bitbake) your image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Finally, when your image is up and running in your custom board you can use the command below to build.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;arm-poky-linux-gnueabi-g++ fileName -o outputFileName&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Dec 2016 16:59:43 GMT</pubDate>
    <dc:creator>Carlos_Musich</dc:creator>
    <dc:date>2016-12-09T16:59:43Z</dc:date>
    <item>
      <title>How to build Native ARM compiler</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-build-Native-ARM-compiler/m-p/658722#M101070</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently, I'm working with i.Mx6 SODIMM custom board. (OS: Linux - Yocto)&lt;/P&gt;&lt;P&gt;There, I want to build the Native ARM compiler to compile my application on my target board itself.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible?&lt;/P&gt;&lt;P&gt;If it so, can any one share the procedure to build that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in Advance.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;J.P.Raja&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Dec 2016 12:01:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-build-Native-ARM-compiler/m-p/658722#M101070</guid>
      <dc:creator>Raana</dc:creator>
      <dc:date>2016-12-08T12:01:25Z</dc:date>
    </item>
    <item>
      <title>Re: How to build Native ARM compiler</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-build-Native-ARM-compiler/m-p/658723#M101071</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raana,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First add the following packet in your &amp;lt;build_dir&amp;gt;/conf/local.conf file&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IMAGE_INSTALL_append += "\&lt;/P&gt;&lt;P&gt;packagegroup-sdk-target \&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The build (bitbake) your image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Finally, when your image is up and running in your custom board you can use the command below to build.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;arm-poky-linux-gnueabi-g++ fileName -o outputFileName&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 16:59:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-build-Native-ARM-compiler/m-p/658723#M101071</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2016-12-09T16:59:43Z</dc:date>
    </item>
  </channel>
</rss>