<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Mars Board booting from eMMC</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Mars-Board-booting-from-eMMC/m-p/658622#M101038</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A href="http://www.forlinx.net"&gt;Forlinx&lt;/A&gt; also has i.MX6Q/DL and i.MX6UL which are all available for booting from eMMC or SD card.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Nov 2016 05:42:22 GMT</pubDate>
    <dc:creator>winy2014</dc:creator>
    <dc:date>2016-11-15T05:42:22Z</dc:date>
    <item>
      <title>Mars Board booting from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mars-Board-booting-from-eMMC/m-p/658621#M101037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;BR /&gt;We are using the Mars board (i.MX6 Dual) for evaluation purpose using the android SDK.&lt;BR /&gt;We are able to flash the u-boot binary on SPI-NOR flash and Kernel and rootFS on eMMC partitions, using the MFG tool provided.&lt;BR /&gt;We are able to boot the Mars board using the above procedure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, we are trying to boot the u-boot binary from the eMMC (tried both on user partition and boot partition).&lt;BR /&gt;But the Mars board is not booted from the eMMC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: We erased the u-boot binary present in the SPI-NOR flash.&lt;BR /&gt;Still, the board is not booted from the eMMC memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reference:&lt;BR /&gt;User Manual : MarS Board User Manual_V1.1.pdf&lt;BR /&gt;MFG tool used : Mfgtools-Rel-12.04.01_ER_MX6Q_UPDATER&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please inform the procedure to boot the Mars board from the eMMC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Arunkumar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Nov 2016 05:17:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mars-Board-booting-from-eMMC/m-p/658621#M101037</guid>
      <dc:creator>arunkumarjts</dc:creator>
      <dc:date>2016-11-15T05:17:32Z</dc:date>
    </item>
    <item>
      <title>Re: Mars Board booting from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mars-Board-booting-from-eMMC/m-p/658622#M101038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A href="http://www.forlinx.net"&gt;Forlinx&lt;/A&gt; also has i.MX6Q/DL and i.MX6UL which are all available for booting from eMMC or SD card.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Nov 2016 05:42:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mars-Board-booting-from-eMMC/m-p/658622#M101038</guid>
      <dc:creator>winy2014</dc:creator>
      <dc:date>2016-11-15T05:42:22Z</dc:date>
    </item>
  </channel>
</rss>