<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Ethernet configuration in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-configuration/m-p/658099#M100945</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please check the connection thoroughly.&lt;BR /&gt;Please try to use another cable, hub, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We checked both eth0 and eth1 interfaces on our i.MX6UL EVK board running Linux demo image and they are working fine.&lt;BR /&gt;We were able to ping the outside.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Mar 2017 04:51:26 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2017-03-17T04:51:26Z</dc:date>
    <item>
      <title>Ethernet configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-configuration/m-p/658098#M100944</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to communicate to the i.mx6UL board using ssh connection from my pc but when i try to connect the Ethernet the terminal shows following msgs&amp;nbsp;&lt;/P&gt;&lt;P&gt;IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready&lt;BR /&gt;fec 20b4000.ethernet eth0: Link is Down&lt;BR /&gt;IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready&lt;BR /&gt;fec 20b4000.ethernet eth0: Link is Up - 10Mbps/Half - flow control off&lt;BR /&gt;IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready&lt;BR /&gt;fec 20b4000.ethernet eth0: Link is Down&lt;BR /&gt;IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready&lt;BR /&gt;fec 20b4000.ethernet eth0: Link is Up - 10Mbps/Half - flow control off&lt;BR /&gt;IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready&lt;BR /&gt;fec 20b4000.ethernet eth0: Link is Down&lt;BR /&gt;IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready&lt;BR /&gt;fec 20b4000.ethernet eth0: Link is Up - 10Mbps/Half - flow control off&lt;BR /&gt;IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready&lt;BR /&gt;fec 20b4000.ethernet eth0: Link is Down&lt;BR /&gt;IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready&lt;BR /&gt;fec 20b4000.ethernet eth0: Link is Up - 10Mbps/Half - flow control off&lt;BR /&gt;IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can anyone please guide me to configure the ethernet connection of this board&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&amp;nbsp;&lt;/P&gt;&lt;P&gt;With Regards&amp;nbsp;&lt;/P&gt;&lt;P&gt;Aditya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Mar 2017 08:57:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ethernet-configuration/m-p/658098#M100944</guid>
      <dc:creator>adityaprajapati</dc:creator>
      <dc:date>2017-03-16T08:57:26Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-configuration/m-p/658099#M100945</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please check the connection thoroughly.&lt;BR /&gt;Please try to use another cable, hub, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We checked both eth0 and eth1 interfaces on our i.MX6UL EVK board running Linux demo image and they are working fine.&lt;BR /&gt;We were able to ping the outside.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Mar 2017 04:51:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ethernet-configuration/m-p/658099#M100945</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2017-03-17T04:51:26Z</dc:date>
    </item>
  </channel>
</rss>