<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Yocto - Image build fails because &amp;quot;nothing RPROVIDES libavresample&amp;quot; in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Image-build-fails-because-quot-nothing-RPROVIDES/m-p/657727#M100893</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to build a custom Yocto image based on core-image-base for my iMX6 based board SECO A62J. I use Hob to do this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After having selected my machine, my layers and my image, I custom my packages list by adding chromium. This automatically select libexif and libav which are Chromium dependencies. The build of the packages is successful&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The last step is the build of the image, and this is where my problem appears. I select the packages I want to include in my image, including Chromium, libexif and libav (and its dependencies).&lt;/P&gt;&lt;P&gt;And I got those errors :&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Nothing RPROVIDES 'libavresample' (but /home/adrien/fsl-release-bsp/build_anna/recipes/images/fsl-image-gui-edited-20170131-144607.bb RDEPENDS on or otherwise requires it)&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;and&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Required build target 'fsl-image-gui-edited-20170131-144607' has no buildable providers.&lt;BR /&gt;Missing or unbuildable dependency chain was: ['fsl-image-gui-edited-20170131-144607', 'libavresample']&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, the library libavresample.so is built successfully and can be found&amp;nbsp; under my build directory in sysroots/"machine_name"/usr/lib/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What am I missing here?&lt;/P&gt;&lt;P&gt;Thank you for your kind help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 31 Jan 2017 14:03:07 GMT</pubDate>
    <dc:creator>adrienfaure</dc:creator>
    <dc:date>2017-01-31T14:03:07Z</dc:date>
    <item>
      <title>Yocto - Image build fails because "nothing RPROVIDES libavresample"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Image-build-fails-because-quot-nothing-RPROVIDES/m-p/657727#M100893</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to build a custom Yocto image based on core-image-base for my iMX6 based board SECO A62J. I use Hob to do this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After having selected my machine, my layers and my image, I custom my packages list by adding chromium. This automatically select libexif and libav which are Chromium dependencies. The build of the packages is successful&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The last step is the build of the image, and this is where my problem appears. I select the packages I want to include in my image, including Chromium, libexif and libav (and its dependencies).&lt;/P&gt;&lt;P&gt;And I got those errors :&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Nothing RPROVIDES 'libavresample' (but /home/adrien/fsl-release-bsp/build_anna/recipes/images/fsl-image-gui-edited-20170131-144607.bb RDEPENDS on or otherwise requires it)&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;and&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Required build target 'fsl-image-gui-edited-20170131-144607' has no buildable providers.&lt;BR /&gt;Missing or unbuildable dependency chain was: ['fsl-image-gui-edited-20170131-144607', 'libavresample']&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, the library libavresample.so is built successfully and can be found&amp;nbsp; under my build directory in sysroots/"machine_name"/usr/lib/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What am I missing here?&lt;/P&gt;&lt;P&gt;Thank you for your kind help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Jan 2017 14:03:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Image-build-fails-because-quot-nothing-RPROVIDES/m-p/657727#M100893</guid>
      <dc:creator>adrienfaure</dc:creator>
      <dc:date>2017-01-31T14:03:07Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto - Image build fails because "nothing RPROVIDES libavresample"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Image-build-fails-because-quot-nothing-RPROVIDES/m-p/657728#M100894</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I’m linking to this same question in an external forum with some insights.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://stackoverflow.com/questions/41964910/yocto-image-build-fails-because-nothing-rprovides-libavresample"&gt;http://stackoverflow.com/questions/41964910/yocto-image-build-fails-because-nothing-rprovides-libavresample&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Feb 2017 21:40:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Image-build-fails-because-quot-nothing-RPROVIDES/m-p/657728#M100894</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2017-02-28T21:40:12Z</dc:date>
    </item>
  </channel>
</rss>