<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックReuse CAN interface for UART communication</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Reuse-CAN-interface-for-UART-communication/m-p/657722#M100891</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a way to re-purpose the two CAN (DB-9) interfaces on i.mx 6solox dev board for UART communication?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Jan 2017 19:49:05 GMT</pubDate>
    <dc:creator>shailendrakarod</dc:creator>
    <dc:date>2017-01-03T19:49:05Z</dc:date>
    <item>
      <title>Reuse CAN interface for UART communication</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reuse-CAN-interface-for-UART-communication/m-p/657722#M100891</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a way to re-purpose the two CAN (DB-9) interfaces on i.mx 6solox dev board for UART communication?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jan 2017 19:49:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reuse-CAN-interface-for-UART-communication/m-p/657722#M100891</guid>
      <dc:creator>shailendrakarod</dc:creator>
      <dc:date>2017-01-03T19:49:05Z</dc:date>
    </item>
    <item>
      <title>Re: Reuse CAN interface for UART communication</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reuse-CAN-interface-for-UART-communication/m-p/657723#M100892</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shailendra&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;muxing options are given in Table 4-1. Pin Assignments i.MX6SX Reference Manual &lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and seems there are no options for uarts.&lt;/P&gt;&lt;P&gt;Schematics (1)&lt;BR /&gt;IMX6SOLOX-SABRESDB-DESIGNFILES&lt;BR /&gt;&lt;A href="http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-board-for-smart-devices-based-on-the-i.mx-6solox-applications-processors:RD-IMX6SX-SABRE?fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-board-for-smart-devices-based-on-the-i.mx-6solox-applications-processors:RD-IMX6SX-SABRE?fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jan 2017 23:58:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reuse-CAN-interface-for-UART-communication/m-p/657723#M100892</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-01-04T23:58:18Z</dc:date>
    </item>
  </channel>
</rss>