<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックReassign Controller Area Network (CAN) interfaces to UART</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Reassign-Controller-Area-Network-CAN-interfaces-to-UART/m-p/657519#M100869</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use the two CAN (DB-9) interfaces on i.mx 6solox development board as UARTs. Is this possible? If yes then can I use these UARTs from M4?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Jan 2017 18:42:54 GMT</pubDate>
    <dc:creator>shailendrakarod</dc:creator>
    <dc:date>2017-01-03T18:42:54Z</dc:date>
    <item>
      <title>Reassign Controller Area Network (CAN) interfaces to UART</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reassign-Controller-Area-Network-CAN-interfaces-to-UART/m-p/657519#M100869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use the two CAN (DB-9) interfaces on i.mx 6solox development board as UARTs. Is this possible? If yes then can I use these UARTs from M4?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jan 2017 18:42:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reassign-Controller-Area-Network-CAN-interfaces-to-UART/m-p/657519#M100869</guid>
      <dc:creator>shailendrakarod</dc:creator>
      <dc:date>2017-01-03T18:42:54Z</dc:date>
    </item>
    <item>
      <title>Re: Reassign Controller Area Network (CAN) interfaces to UART</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reassign-Controller-Area-Network-CAN-interfaces-to-UART/m-p/657520#M100870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shailendra&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/441946"&gt;Reuse CAN interface for UART communication&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;both cores can access modules if RDC is configured properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jan 2017 03:39:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reassign-Controller-Area-Network-CAN-interfaces-to-UART/m-p/657520#M100870</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-01-06T03:39:29Z</dc:date>
    </item>
  </channel>
</rss>