<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How does M4 and A9 on i.mx6sx access DDR</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657409#M100830</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have doubt with the QoS. If the QoS says the priority of the Master, why the PL301 has two arbitration schemes (LGR and RR)? Besides, I not able to find which one is the default one.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11744i386101253BA4F76F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Jan 2017 08:50:30 GMT</pubDate>
    <dc:creator>imanolallende</dc:creator>
    <dc:date>2017-01-17T08:50:30Z</dc:date>
    <item>
      <title>How does M4 and A9 on i.mx6sx access DDR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657403#M100824</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In my i.mx6sx sdb board,there is only a DDR3(1G),How can I allocate some memory(such as 200M) as shared memory ? How dose M4 and A9 access the shared memory I allocated?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jan 2017 03:20:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657403#M100824</guid>
      <dc:creator>jingyangxie</dc:creator>
      <dc:date>2017-01-04T03:20:05Z</dc:date>
    </item>
    <item>
      <title>Re: How does M4 and A9 on i.mx6sx access DDR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657404#M100825</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jingyang xie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First look at Figure 43-1. NIC-301 Bus System. This drawing does have a couple of flaws: The dark blue box labeled ENET connected to the light blue box labeled Main should actually be a light blue box. The light blue boxes represent bus switches that route signals along AXI buses. Also, the Cortex A9 core in a dark blue box should connect directly to the Main switch. Ignore the top line of that page. There are seven switches, not five and the five listed are not the correct names (left over from i.MX6Q).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So what to do with this knowledge. The Table 43-6 QoS and tidemark parameters provide the "Quality of Service" values that are assigned to traffic as they enter the NIC-301 system. The switch M4 has 3 port listings: M4-0 and M4-1 are both assigned a QOS value of "2", by default. The gpv6 port goes to the Wakeup switch and is not important to this discussion. Then comes the Switch Main which has nine ports assigned. The two ports for A9-0 and A9-1 are the AXI buses to the A9 core. The are assigned a QoS factor of "0". There is also a port connecting the Main switch to the M4 switch. It has a QoS of "0", but that does not mean that traffic coming from the M4 gets its QoS reassigned to "0". The original QoS factor stays with the traffic throughout its lifetime.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then, if you go to section 40.5.1.3 Dynamic scoring mode, you will see a discussion of how the MMDC will score and service traffic requests. It should be reasonably self explanatory. A higher score results in higher priority, so the QoS assigned by the NIC to M4 gives it an edge over the A9 core (except that the MMDC traffic from the M4 core does have to go through one extra switch than the A9 core for a little extra travel time).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The QoS values assigned by the NIC can be changed. First you need the base address of the appropriate NIC listed in Table 43-2. CM4 GPV ports memory allocations (see note below). For the M4 port, the base address starts at 0x41100000. Then look at Table 43-6 for the port number on the M4 switch: M4-0 = 66 and M4-1 =67. multiply that number by 0x1000 to get the start address for that port. Example: M4-0 = 66, so the setting for this port are stored at 0x41100000 + 66*0x1000 is 0x41142000. Then use the offsets from Table 43-5 to find the register address of the desired QoS score. There are two: One for Read accesses and one for Write accesses.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NOTE: If you look in the reference manual you will see a similar table Table 43-1 CA9 GPV ports memory allocations with different addresses. Even though they have different addresses, they access the same information from within the single AIPS table storage location. So if you set the QoS value using the registers for the M4 core (bit-30 = 'b1), the A9 core will find the same information using an address in which bit-30 = 'b0.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jan 2017 22:57:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657404#M100825</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2017-01-04T22:57:57Z</dc:date>
    </item>
    <item>
      <title>Re: How does M4 and A9 on i.mx6sx access DDR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657405#M100826</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,Carlos&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Thanks for your prompt reply.But It's a bit complicated for me,Can you give me some example apps ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PS : My intention is to allocate some memory form DDR3,and A9 can write data in the memory,M4 can read the data from the same memory.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jan 2017 01:28:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657405#M100826</guid>
      <dc:creator>jingyangxie</dc:creator>
      <dc:date>2017-01-05T01:28:31Z</dc:date>
    </item>
    <item>
      <title>Re: How does M4 and A9 on i.mx6sx access DDR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657406#M100827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jingyang xie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can take a look to &lt;SPAN style="font-size: 11.0pt;"&gt;RPMsg&lt;/SPAN&gt; with FreeRTOS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can download FreeRTOS for IMx6SX here:&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;A href="http://www.nxp.com/imx6SX"&gt;http://www.nxp.com/imx6SX&lt;/A&gt; &amp;gt; Software &amp;amp; Tools tab&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;FreeRTOS™ BSP 1.0.1 for the i.MX 6SoloX ARM® Cortex®-M4 core&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;You will need the following documentation:&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;STRONG&gt;i.MX_Linux_User's_Guide.pdf&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;3 Basic Terminal Setup&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;The USB to serial driver can be found under &lt;A href="http://www.ftdichip.com/Drivers/VCP.htm"&gt;www.ftdichip.com/Drivers/VCP.htm&lt;/A&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;STRONG&gt;i.MX_Linux_Reference_Manual.pdf&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;51 Remote Processor Messaging (RPMsg)&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;STRONG&gt;Getting_Started_with_FreeRTOS_BSP_for_i.MX_6SoloX.pdf&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;6 Running Application with U-Boot&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;STRONG&gt;FreeRTOS_BSP_for_i.MX_6SoloX_Demo_User’s_Guide.pdf&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;10 RPMsg Ping-Pong FreeRTOS Demo with RTOS API&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Once you installed FreeRTOS build rpmsg demos to generate .bin file. E.g. &lt;SPAN style="font-size: 11.0pt;"&gt;C:\NXP\FreeRTOS_BSP_1.0.1_iMX6SX\examples\imx6sx_sdb_m4\demo_apps\rpmsg\pingpong_freertos\&amp;lt;compiler&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Then boot in A9 core and stop in uboot to configure the M4 application. I have made in 2 different ways:&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;ONE&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;env default -a&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;setenv fdt_file imx6sx-sdb-m4.dtb&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;setenv m4image 'rpmsg_pingpong_freertos_example.bin'&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;setenv run_m4_tcm 'if run loadm4image; then cp.b ${loadaddr} 0x7f8000 0x8000; bootaux 0x7f8000; fi'&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;setenv bootcmd "run run_m4_tcm;${bootcmd}"&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;setenv mmcargs "${mmcargs} uart_from_osc"&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;saveenv&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;boot&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;TWO&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;env default –a&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;setenv m4image 'rpmsg_pingpong_freertos_example.bin'&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;setenv fdt_file imx6sx-sdb-m4.dtb&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;setenv bootcmd "run m4boot;${bootcmd}"&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;setenv mmcargs "${mmcargs} uart_from_osc"&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;run update_m4_from_sd&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;saveenv&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;boot&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Finally launch M4 application from A9 cmd:&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;$ cd /lib/modules/4.1.15-1.2.0+g77f6154/kernel/drivers/rpmsg&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;$ insmod imx_rpmsg_pingpong.ko&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;$ rmmod imx_rpmsg_pingpong&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jan 2017 23:02:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657406#M100827</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2017-01-05T23:02:10Z</dc:date>
    </item>
    <item>
      <title>Re: How does M4 and A9 on i.mx6sx access DDR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657407#M100828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Anyone knows?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jan 2017 01:47:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657407#M100828</guid>
      <dc:creator>jingyangxie</dc:creator>
      <dc:date>2017-01-06T01:47:55Z</dc:date>
    </item>
    <item>
      <title>Re: How does M4 and A9 on i.mx6sx access DDR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657408#M100829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jingyang,&amp;nbsp; Hello Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have&amp;nbsp; similar need for a 16MB shared space but using the i.MX7D.&amp;nbsp; I built the rpmsg examples and they're great for what they are - a pingpong exchange and string echo.&amp;nbsp; The maximum size allowed in the reference FreeRTOS rpmsg implementation is 512 bytes (.../middleware/multicore/open-amp/rpmsg/rpmsg_core.h line 44, RPMSG_BUFFER_SIZE definition).&amp;nbsp; It seems doubtful that buffer size can be increased to 16 or 200MB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am looking at using a device tree reserved-memory object to define and access a shared memory block.&amp;nbsp; See&amp;nbsp; linux rel_imx_4.1.15_1.1.0_ga/arch/arm/boot/dts/imx6sx.dtsi for example defining a shared-dma-pool.&amp;nbsp; Access could be managed using the Messaging Unit or other cooperative method.&amp;nbsp; Is this a viable approach?&amp;nbsp; The iMX7D DRM Section 4.3.3.3.2 provides a high level description as "Passing fixed-length data"; Section 4.3.3.8 and 4.3.3.9 discuss interrupt-based methodologies for access control.&amp;nbsp; Does an example implementation exist?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&amp;nbsp;&amp;nbsp; Joe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jan 2017 22:30:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657408#M100829</guid>
      <dc:creator>jtheath</dc:creator>
      <dc:date>2017-01-09T22:30:26Z</dc:date>
    </item>
    <item>
      <title>Re: How does M4 and A9 on i.mx6sx access DDR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657409#M100830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have doubt with the QoS. If the QoS says the priority of the Master, why the PL301 has two arbitration schemes (LGR and RR)? Besides, I not able to find which one is the default one.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11744i386101253BA4F76F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jan 2017 08:50:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657409#M100830</guid>
      <dc:creator>imanolallende</dc:creator>
      <dc:date>2017-01-17T08:50:30Z</dc:date>
    </item>
    <item>
      <title>Re: How does M4 and A9 on i.mx6sx access DDR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657410#M100831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joe,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;as you can see in&amp;nbsp;&lt;STRONG&gt;Table 2-1. System memory map&lt;/STRONG&gt; and &lt;STRONG&gt;Table 2-2. CM4 memory map, &lt;/STRONG&gt;there are 1536MB available as shared memory at address 0x80000000 which is for the&amp;nbsp;MMDC x32DDR Controller.&lt;STRONG&gt; &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may edit the RPMsg demo application to allocate and initialize the RPMsg driver resources in this area. You may find RPMsg APIS in RPMsg RTOS Layer User’s Guide (RPMsg_RTOS_Layer_User’s_Guide.pdf).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jan 2017 23:30:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657410#M100831</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2017-01-18T23:30:26Z</dc:date>
    </item>
    <item>
      <title>Re: How does M4 and A9 on i.mx6sx access DDR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657411#M100832</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've reviewed the rpmsg implementations in both the FreeRTOS and Linux code bases.&amp;nbsp; Both define the used buffer size to 512 bytes, with Linux allocating 512 such buffers for a total of 256KB.&amp;nbsp; I need to push a few MBs of control info from the A7 through the M4.&amp;nbsp; It doesn't look like rpmsg is built for that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have defined a 16MB block as reserved-memory and can access it from the A7 and M4.&amp;nbsp; Is there some mechanism one can use to force the relevant core cache flush and then indicate the flush is complete to the other core?&amp;nbsp; Something akin to using the vertical blanking interval for video frame updates?&amp;nbsp; At the moment it appears the M4 "misses" some memory updates 64 bytes at a time (I have the M4 continually reading memory blocks and dumping the contents).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&amp;nbsp;&amp;nbsp; Joe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jan 2017 23:41:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657411#M100832</guid>
      <dc:creator>jtheath</dc:creator>
      <dc:date>2017-01-18T23:41:43Z</dc:date>
    </item>
    <item>
      <title>Re: How does M4 and A9 on i.mx6sx access DDR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657412#M100833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joe,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't see a direct way to indicate a core that the other core flushed cache. You may interrupt the other core when cache is flushed or use a message which would be the same process but in a higher layer using FreeRTOS services.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jan 2017 18:33:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657412#M100833</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2017-01-19T18:33:58Z</dc:date>
    </item>
    <item>
      <title>Re: How does M4 and A9 on i.mx6sx access DDR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657413#M100834</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, I can figure out a way to signal, e.g. MU_ACR/MU_BCR or another mechanism.&amp;nbsp; It doesn't appear that the "standard" Linux cacheflush() call is available.&amp;nbsp; Is there another call which should be used?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When loading the M4 using u-boot we issue a "dcache flush" command.&amp;nbsp; I tracked that functionality down into arch/arm/cpu/armv7/cmd_m4boot.c.&amp;nbsp; Where does this capability live in the Linux tree?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All the best,&amp;nbsp;&amp;nbsp; Joe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jan 2017 23:30:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657413#M100834</guid>
      <dc:creator>jtheath</dc:creator>
      <dc:date>2017-01-19T23:30:43Z</dc:date>
    </item>
    <item>
      <title>Re: How does M4 and A9 on i.mx6sx access DDR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657414#M100835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi，Joseph&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Could you tell me how can the M4 access&amp;nbsp;&lt;SPAN style="display: inline !important; float: none; background-color: transparent; color: #51626f; font-family: 'Helvetica Neue',Helvetica,Arial,'Lucida Grande',sans-serif; font-size: 15px; font-style: normal; font-variant: normal; font-weight: 400; letter-spacing: normal; orphans: 2; text-align: left; text-decoration: none; text-indent: 0px; text-transform: none; -webkit-text-stroke-width: 0px; white-space: normal; word-spacing: 0px;"&gt;a device tree reserved-memory ？&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 May 2018 09:36:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657414#M100835</guid>
      <dc:creator>jingyangxie</dc:creator>
      <dc:date>2018-05-17T09:36:18Z</dc:date>
    </item>
    <item>
      <title>Re: How does M4 and A9 on i.mx6sx access DDR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657415#M100836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i.MX Development Miscellanea(i.MX 开发杂记)&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-335198"&gt;https://community.nxp.com/docs/DOC-335198&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX6SX_M4_MPU_Settings_For_RPMSG_04132018.pdf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jun 2018 08:11:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657415#M100836</guid>
      <dc:creator>BiyongSUN</dc:creator>
      <dc:date>2018-06-08T08:11:55Z</dc:date>
    </item>
    <item>
      <title>Re: How does M4 and A9 on i.mx6sx access DDR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657416#M100837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;M4 is the same way to use address to access the Linux reserved memory. Reserve just let Linux don't destroy the memory for M4.&amp;nbsp; If the memory is for M4 only, you can use M4 to configure cacheable to make it fast. But for rpmsg. has to be non cacheable.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jun 2018 08:16:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657416#M100837</guid>
      <dc:creator>BiyongSUN</dc:creator>
      <dc:date>2018-06-08T08:16:24Z</dc:date>
    </item>
    <item>
      <title>Re: How does M4 and A9 on i.mx6sx access DDR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657417#M100838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,Sun&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Do you know why doesnot the IMX6SXRM talk about&amp;nbsp; MPU for M4 in details？The resigters for MPU in FreeRTOS porject can not be found in IMX6SXRM&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jun 2018 01:42:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-does-M4-and-A9-on-i-mx6sx-access-DDR/m-p/657417#M100838</guid>
      <dc:creator>jingyangxie</dc:creator>
      <dc:date>2018-06-11T01:42:36Z</dc:date>
    </item>
  </channel>
</rss>