<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Yocto and OpenCV 3</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-and-OpenCV-3/m-p/656688#M100662</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello yoramshacham,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You will find the following packaged which you can add with IMAGE_INSTALL_APPEND on the local.conf file. Alternatively you can bake them separatedly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, these are for OpenCV 2.4 on the L4.1.15 BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can find OpenCV 3.1 on the krogoth branch of the Community BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;opencv - for building opencv&lt;/P&gt;&lt;P&gt;opencv-samples for building the samples.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Sep 2016 21:32:45 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2016-09-27T21:32:45Z</dc:date>
    <item>
      <title>Yocto and OpenCV 3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-and-OpenCV-3/m-p/656687#M100661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there an integration for OpenCV 3 in Yocto ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Sep 2016 14:17:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-and-OpenCV-3/m-p/656687#M100661</guid>
      <dc:creator>yoramshacham</dc:creator>
      <dc:date>2016-09-27T14:17:14Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto and OpenCV 3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-and-OpenCV-3/m-p/656688#M100662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello yoramshacham,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You will find the following packaged which you can add with IMAGE_INSTALL_APPEND on the local.conf file. Alternatively you can bake them separatedly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, these are for OpenCV 2.4 on the L4.1.15 BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can find OpenCV 3.1 on the krogoth branch of the Community BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;opencv - for building opencv&lt;/P&gt;&lt;P&gt;opencv-samples for building the samples.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Sep 2016 21:32:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-and-OpenCV-3/m-p/656688#M100662</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-09-27T21:32:45Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto and OpenCV 3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-and-OpenCV-3/m-p/656689#M100663</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;gusarambula,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the prompt reply.&lt;BR /&gt;I already have OpenCV 2.4 running on both my iMX6UL and iMX6DL.&lt;/P&gt;&lt;P&gt;I see some performance issues in objdetect (same as I saw on Ubuntu desktop before moving to OpenCV 3).&lt;/P&gt;&lt;P&gt;Being new to this, can you please elaborate how I find it there, download, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks :-)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Sep 2016 08:32:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-and-OpenCV-3/m-p/656689#M100663</guid>
      <dc:creator>yoramshacham</dc:creator>
      <dc:date>2016-09-28T08:32:12Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto and OpenCV 3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-and-OpenCV-3/m-p/656690#M100664</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello yoramshacham,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you wish to test OpenCV 3.1 then definitely try using the krogoth branch of the Community BSP.&lt;/P&gt;&lt;P&gt;If you are new to Yocto check the following training:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-94035"&gt;https://community.nxp.com/docs/DOC-94035&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Only use git below instead:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;repo init -u &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fgithub.com%2FFreescale%2Ffsl-community-bsp-platform" rel="nofollow" target="_blank"&gt;https://github.com/Freescale/fsl-community-bsp-platform&lt;/A&gt;&lt;SPAN&gt; -b krogoth&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You would need to add the OpenCV packages, which can be done by adding the following lines to your local.conf file (you will see this a bit more explained on the training)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IMAGE_INSTALL_append += “ opencv opencv-samples”&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Sep 2016 15:28:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-and-OpenCV-3/m-p/656690#M100664</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-09-30T15:28:23Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto and OpenCV 3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-and-OpenCV-3/m-p/1391928#M185012</link>
      <description>&lt;P&gt;ok new L5.10.52 all have lah or u put this :&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;IMAGE_INSTALL_append += “ opencv opencv-samples”&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;b.r.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 09 Jan 2022 12:31:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-and-OpenCV-3/m-p/1391928#M185012</guid>
      <dc:creator>josephzhou1</dc:creator>
      <dc:date>2022-01-09T12:31:35Z</dc:date>
    </item>
  </channel>
</rss>