<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic About UVC camera in AndroidM6.0 for MX6Q-SABRE board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/About-UVC-camera-in-AndroidM6-0-for-MX6Q-SABRE-board/m-p/656181#M100561</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We run AndroidM6.0 demo image on MX6Q-SABRE board.&lt;BR /&gt;&amp;nbsp; - Board: MX6Q-SABRE-SD&lt;BR /&gt;&amp;nbsp; - Image: android_M6.0.1_2.0.0_image_6dqpsabresd&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We try UVC (USB Video Class) camera input.&lt;BR /&gt;However, the USB camera is not recognized.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the Release Notes(Rev. M6.0.1_2.0.0, 06/2016), BSP supports Media – USB Camera(Logitech(C250 / E3500)).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does this pre-build image support the USB Camera?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition, camera application is not included in this image.&lt;BR /&gt;Would you tell me the available camera application for this image?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Yuuki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Sep 2016 03:58:42 GMT</pubDate>
    <dc:creator>yuuki</dc:creator>
    <dc:date>2016-09-28T03:58:42Z</dc:date>
    <item>
      <title>About UVC camera in AndroidM6.0 for MX6Q-SABRE board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-UVC-camera-in-AndroidM6-0-for-MX6Q-SABRE-board/m-p/656181#M100561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We run AndroidM6.0 demo image on MX6Q-SABRE board.&lt;BR /&gt;&amp;nbsp; - Board: MX6Q-SABRE-SD&lt;BR /&gt;&amp;nbsp; - Image: android_M6.0.1_2.0.0_image_6dqpsabresd&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We try UVC (USB Video Class) camera input.&lt;BR /&gt;However, the USB camera is not recognized.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the Release Notes(Rev. M6.0.1_2.0.0, 06/2016), BSP supports Media – USB Camera(Logitech(C250 / E3500)).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does this pre-build image support the USB Camera?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition, camera application is not included in this image.&lt;BR /&gt;Would you tell me the available camera application for this image?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Yuuki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Sep 2016 03:58:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-UVC-camera-in-AndroidM6-0-for-MX6Q-SABRE-board/m-p/656181#M100561</guid>
      <dc:creator>yuuki</dc:creator>
      <dc:date>2016-09-28T03:58:42Z</dc:date>
    </item>
    <item>
      <title>Re: About UVC camera in AndroidM6.0 for MX6Q-SABRE board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-UVC-camera-in-AndroidM6-0-for-MX6Q-SABRE-board/m-p/656182#M100562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I’m sorry to be pressing.&lt;BR /&gt;Do you have information about this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Yuuki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2016 01:27:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-UVC-camera-in-AndroidM6-0-for-MX6Q-SABRE-board/m-p/656182#M100562</guid>
      <dc:creator>yuuki</dc:creator>
      <dc:date>2016-10-12T01:27:03Z</dc:date>
    </item>
    <item>
      <title>Re: About UVC camera in AndroidM6.0 for MX6Q-SABRE board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-UVC-camera-in-AndroidM6-0-for-MX6Q-SABRE-board/m-p/656183#M100563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi yuuki,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In prebuilt image, USB UVC class camera is supported, you should be able to use on console with gstreamer command..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please there are some issues regarding camera on SDP board, please check the attached document.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Oct 2016 15:04:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-UVC-camera-in-AndroidM6-0-for-MX6Q-SABRE-board/m-p/656183#M100563</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2016-10-18T15:04:35Z</dc:date>
    </item>
  </channel>
</rss>