<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: About GPIO input and interrupt</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/About-GPIO-input-and-interrupt/m-p/654547#M100248</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Soichi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes one can use the input port and the interrupt function together with the i.MX6 pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 31 Jan 2017 00:13:59 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-01-31T00:13:59Z</dc:date>
    <item>
      <title>About GPIO input and interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-GPIO-input-and-interrupt/m-p/654546#M100247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will ask about i.MX6 Quad.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="margin: 0in; font-family: 'ＭＳ Ｐゴシック'; font-size: 9.0pt;"&gt;Can I use the input port and the interrupt function together with the i.MX6 pin?&lt;/P&gt;&lt;P style="margin: 0in; font-family: 'ＭＳ Ｐゴシック'; font-size: 9.0pt;"&gt;In the microcomputer used in the past, the terminal using the interrupt function could not be read as a normal input port, so I asked a question.&lt;/P&gt;&lt;P style="margin: 0in; font-family: 'ＭＳ Ｐゴシック'; font-size: 9.0pt;"&gt;&lt;/P&gt;&lt;P style="margin: 0in; font-family: 'ＭＳ Ｐゴシック'; font-size: 9.0pt;"&gt;Best Regards,&lt;/P&gt;&lt;P style="margin: 0in; font-family: 'ＭＳ Ｐゴシック'; font-size: 9.0pt;"&gt;soichi/avnet&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jan 2017 10:13:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-GPIO-input-and-interrupt/m-p/654546#M100247</guid>
      <dc:creator>soichiyamamoto</dc:creator>
      <dc:date>2017-01-30T10:13:08Z</dc:date>
    </item>
    <item>
      <title>Re: About GPIO input and interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-GPIO-input-and-interrupt/m-p/654547#M100248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Soichi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes one can use the input port and the interrupt function together with the i.MX6 pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Jan 2017 00:13:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-GPIO-input-and-interrupt/m-p/654547#M100248</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-01-31T00:13:59Z</dc:date>
    </item>
  </channel>
</rss>