<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6Q - boot from eMMC in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-boot-from-eMMC/m-p/654375#M100234</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Abdulaziz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can debug it using procedure described in&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/thread/307723"&gt;https://community.freescale.com/thread/307723&lt;/A&gt;&lt;/P&gt;&lt;P&gt;after fail attach jtag and check boot mode in register SRC_SBMR1,&lt;/P&gt;&lt;P&gt;check if &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;ROM puts boot data at 0x907400&lt;/SPAN&gt;. Check with oscilloscope emmc&lt;/P&gt;&lt;P&gt;lines. Sd image should work for emmc too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Apr 2017 23:26:53 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-04-06T23:26:53Z</dc:date>
    <item>
      <title>IMX6Q - boot from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-boot-from-eMMC/m-p/654374#M100233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, we have Imx6qsabre-sd based custom board, with ram 2 gb micron Ram and 4gb Micron eMMC. It can boot from sd card with our yocto image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We want to boot from eMMC, in order to achieve this I have tried two&amp;nbsp;method mainly:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) I can write our yocto *****.sdcard image(same image with sdcard image) into eMMC with sdcard boot, but when I configure switches (1-2-4-6-7 on) it does not start from eMMC.&lt;/P&gt;&lt;P&gt;2) When I write u-boot.imx, dtb file, zImage and rootfs of sdcard image using Mfgtool, It does not boot from eMMC when I made switch configurations. In both try, It goes into download mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As far as I see, for both methods, partition sizes and start points differs from each other. Mfgtool work with imx6qpsabre-sd board fine and mksdcard.sh is same for all boards in Mfgtool, so its partition sizes should be true. I did not make any configuration on yocto layers for boot from eMMC, I am using same resources of sdcard. Is there any configurations for yocto or u-boot-fscl? In addition to this, when I write UBOOT_CONFIG = "emmc" into the local.conf file yocto does not generate u-boot.imx image. How should be partiton table for eMMC and what is jump address of rom.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Apr 2017 13:24:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-boot-from-eMMC/m-p/654374#M100233</guid>
      <dc:creator>aydogmus</dc:creator>
      <dc:date>2017-04-06T13:24:20Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q - boot from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-boot-from-eMMC/m-p/654375#M100234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Abdulaziz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can debug it using procedure described in&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/thread/307723"&gt;https://community.freescale.com/thread/307723&lt;/A&gt;&lt;/P&gt;&lt;P&gt;after fail attach jtag and check boot mode in register SRC_SBMR1,&lt;/P&gt;&lt;P&gt;check if &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;ROM puts boot data at 0x907400&lt;/SPAN&gt;. Check with oscilloscope emmc&lt;/P&gt;&lt;P&gt;lines. Sd image should work for emmc too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Apr 2017 23:26:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-boot-from-eMMC/m-p/654375#M100234</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-04-06T23:26:53Z</dc:date>
    </item>
  </channel>
</rss>