<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Loop back of Display output data to CSI inputs</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Loop-back-of-Display-output-data-to-CSI-inputs/m-p/654097#M100152</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Harish&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems lvds is not compatible with mipi-dphy,&lt;/P&gt;&lt;P&gt;both mipi dsi and csi have mipi-dphy and can be connected together.&lt;/P&gt;&lt;P&gt;However timings and protocols are different so seems this also not possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 30 Apr 2017 23:14:06 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-04-30T23:14:06Z</dc:date>
    <item>
      <title>Loop back of Display output data to CSI inputs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Loop-back-of-Display-output-data-to-CSI-inputs/m-p/654096#M100151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;We are using IMX6 Quad based COM for one of our end application,need info on whether it is possible to loop back LVDS Display or MIPI DSI outputs from the processor to MIPI CSI for validation of CSI interaface in our end application with some test data.&lt;/P&gt;&lt;P&gt;Need also some first hand information on data format compatibility between these interfaces.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Apr 2017 09:44:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Loop-back-of-Display-output-data-to-CSI-inputs/m-p/654096#M100151</guid>
      <dc:creator>harishs</dc:creator>
      <dc:date>2017-04-29T09:44:39Z</dc:date>
    </item>
    <item>
      <title>Re: Loop back of Display output data to CSI inputs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Loop-back-of-Display-output-data-to-CSI-inputs/m-p/654097#M100152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Harish&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems lvds is not compatible with mipi-dphy,&lt;/P&gt;&lt;P&gt;both mipi dsi and csi have mipi-dphy and can be connected together.&lt;/P&gt;&lt;P&gt;However timings and protocols are different so seems this also not possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 30 Apr 2017 23:14:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Loop-back-of-Display-output-data-to-CSI-inputs/m-p/654097#M100152</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-04-30T23:14:06Z</dc:date>
    </item>
  </channel>
</rss>