<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMXQP SD Boot Issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMXQP-SD-Boot-Issue/m-p/653380#M100034</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kishor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check if clocks are stable (24MHz crystal, 32.768KHz) and try&lt;/P&gt;&lt;P&gt;to extend POR up to 0.8-1 sec. Also may be recommended to check power supplies,&lt;/P&gt;&lt;P&gt;are they are stable when POR released, some hints may found in i.MX6 System Development User’s&lt;/P&gt;&lt;P&gt;Guide Chapter 8 Avoiding Board Bring-up Problems&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fuser_guide%2FIMX6DQ6SDLHDG.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Feb 2017 01:20:37 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-02-21T01:20:37Z</dc:date>
    <item>
      <title>IMXQP SD Boot Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXQP-SD-Boot-Issue/m-p/653379#M100033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are observing SD Boot Issue on IMX6QP based custom hardware board. We have the below &lt;/P&gt;&lt;P&gt;SD BOOT Configuration&lt;BR /&gt;SRC_SBMR1(0x020d8004) = 0x00001040&lt;BR /&gt;SRC_SBMR2(0x020d801c) = 0x12000001&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On POR, SD boot is not happening.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when we boot from eMMC, run "mmc dev 1" the SD card returns the message: "Card did not respond to voltage select"&lt;/P&gt;&lt;P&gt;At this time if we plug out the SD card and plug in and execute "mmc dev 1" the SD cards gets detected.&lt;/P&gt;&lt;P&gt;After the card is detected if we reset the board (not POR) after installing jumpers for SD boot we could see SD boot working.&lt;/P&gt;&lt;P&gt;But if we do POR the SD boot is not working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Based on this behavior we are suspecting that ROM code is unable to access the SD card for some reason?&lt;/P&gt;&lt;P&gt;Appreciate if anyone have any inputs on this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Kishor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Feb 2017 19:11:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXQP-SD-Boot-Issue/m-p/653379#M100033</guid>
      <dc:creator>kishorr</dc:creator>
      <dc:date>2017-02-20T19:11:53Z</dc:date>
    </item>
    <item>
      <title>Re: IMXQP SD Boot Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXQP-SD-Boot-Issue/m-p/653380#M100034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kishor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check if clocks are stable (24MHz crystal, 32.768KHz) and try&lt;/P&gt;&lt;P&gt;to extend POR up to 0.8-1 sec. Also may be recommended to check power supplies,&lt;/P&gt;&lt;P&gt;are they are stable when POR released, some hints may found in i.MX6 System Development User’s&lt;/P&gt;&lt;P&gt;Guide Chapter 8 Avoiding Board Bring-up Problems&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fuser_guide%2FIMX6DQ6SDLHDG.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Feb 2017 01:20:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXQP-SD-Boot-Issue/m-p/653380#M100034</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-02-21T01:20:37Z</dc:date>
    </item>
  </channel>
</rss>