<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is there any yocto branch which support destop on imx5/6 serial reference boards in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-there-any-yocto-branch-which-support-destop-on-imx5-6-serial/m-p/653343#M100027</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I compared the ltb build with ubuntu10.04 version with bitbake fsl-machine-test. &amp;nbsp;fsl-machine-test one donot including the ipu,vpu and gpu drivers, is only start the uart console with tty. Does somebody know the patches for the gpu,vpu,ipu I need to perform or where can I get it ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks!&lt;/P&gt;&lt;P&gt;wenming&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Sep 2016 14:08:07 GMT</pubDate>
    <dc:creator>wenmingfeng</dc:creator>
    <dc:date>2016-09-28T14:08:07Z</dc:date>
    <item>
      <title>Is there any yocto branch which support destop on imx5/6 serial reference boards</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-there-any-yocto-branch-which-support-destop-on-imx5-6-serial/m-p/653342#M100026</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on upgrading the kernel from 2.6x to 4.x for our imx535 projects. I am now can build the uboot,kernel from yocto, but the ubuntu desktop will not started with my mx53qsb reference board. somebody has suggestions and shares about how to build or porting a desktop like ubuntu to imx5/6 or there is already one please inform me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks!&lt;BR /&gt;Wenming&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Sep 2016 21:02:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-there-any-yocto-branch-which-support-destop-on-imx5-6-serial/m-p/653342#M100026</guid>
      <dc:creator>wenmingfeng</dc:creator>
      <dc:date>2016-09-26T21:02:03Z</dc:date>
    </item>
    <item>
      <title>Re: Is there any yocto branch which support destop on imx5/6 serial reference boards</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-there-any-yocto-branch-which-support-destop-on-imx5-6-serial/m-p/653343#M100027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I compared the ltb build with ubuntu10.04 version with bitbake fsl-machine-test. &amp;nbsp;fsl-machine-test one donot including the ipu,vpu and gpu drivers, is only start the uart console with tty. Does somebody know the patches for the gpu,vpu,ipu I need to perform or where can I get it ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks!&lt;/P&gt;&lt;P&gt;wenming&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Sep 2016 14:08:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-there-any-yocto-branch-which-support-destop-on-imx5-6-serial/m-p/653343#M100027</guid>
      <dc:creator>wenmingfeng</dc:creator>
      <dc:date>2016-09-28T14:08:07Z</dc:date>
    </item>
    <item>
      <title>Re: Is there any yocto branch which support destop on imx5/6 serial reference boards</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-there-any-yocto-branch-which-support-destop-on-imx5-6-serial/m-p/653344#M100028</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;one can try to build fsl-image-qt5 which Builds an opensource Qt 5 image. These images are only&lt;BR /&gt;supported for i.MX SoC with hardware graphics. They are not supported on the i.MX 6UltraLite and i.MX 7Dual.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Sep 2016 09:03:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-there-any-yocto-branch-which-support-destop-on-imx5-6-serial/m-p/653344#M100028</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2016-09-29T09:03:49Z</dc:date>
    </item>
    <item>
      <title>Re: Is there any yocto branch which support destop on imx5/6 serial reference boards</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-there-any-yocto-branch-which-support-destop-on-imx5-6-serial/m-p/653345#M100029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Joan,&lt;/P&gt;&lt;P&gt;Thanks a lot. which branch has the fsl-image-qt5, I am using the master, it seems not on master branch.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Sep 2016 13:56:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-there-any-yocto-branch-which-support-destop-on-imx5-6-serial/m-p/653345#M100029</guid>
      <dc:creator>wenmingfeng</dc:creator>
      <dc:date>2016-09-29T13:56:50Z</dc:date>
    </item>
  </channel>
</rss>