<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX95 Arm Mali-G310 GPU benchmarking in i.MX Graphics</title>
    <link>https://community.nxp.com/t5/i-MX-Graphics/iMX95-Arm-Mali-G310-GPU-benchmarking/m-p/2204321#M991</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254342"&gt;@Cerviik&lt;/a&gt;,&amp;nbsp;&lt;BR /&gt;Great observation. NXP likely ran GFXBench and Antutu on Android builds for the same Arm-based hardware, not native Linux. These benchmarks are Android-compatible and often used to showcase GPU performance even if the target OS for deployment is Linux.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Jill Muncy&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 13 Nov 2025 09:06:47 GMT</pubDate>
    <dc:creator>jill598muncy</dc:creator>
    <dc:date>2025-11-13T09:06:47Z</dc:date>
    <item>
      <title>iMX95 Arm Mali-G310 GPU benchmarking</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/iMX95-Arm-Mali-G310-GPU-benchmarking/m-p/2189780#M961</link>
      <description>&lt;P&gt;Hello all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I may be missing something, but how come the NXP is showing results of GPU benchmarks from GFXBench and Antutu if none of these has version for Linux Arm?&lt;/P&gt;&lt;P&gt;I am reffering to document E1R05_Prior_NXP_2024.pdf&lt;/P&gt;&lt;P&gt;My understanding is that Arm Mali-G310 is desgin, which is only available with Arm architecture, so these two just dont add up.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can somebody please explain?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&amp;nbsp;&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;</description>
      <pubDate>Tue, 21 Oct 2025 08:23:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/iMX95-Arm-Mali-G310-GPU-benchmarking/m-p/2189780#M961</guid>
      <dc:creator>Cerviik</dc:creator>
      <dc:date>2025-10-21T08:23:55Z</dc:date>
    </item>
    <item>
      <title>Re: iMX95 Arm Mali-G310 GPU benchmarking</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/iMX95-Arm-Mali-G310-GPU-benchmarking/m-p/2191039#M962</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254342"&gt;@Cerviik&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;GFXBench we have it for Linux.&lt;/P&gt;
&lt;P&gt;Antutu is for Android only.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 23 Oct 2025 00:20:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/iMX95-Arm-Mali-G310-GPU-benchmarking/m-p/2191039#M962</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2025-10-23T00:20:54Z</dc:date>
    </item>
    <item>
      <title>Re: iMX95 Arm Mali-G310 GPU benchmarking</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/iMX95-Arm-Mali-G310-GPU-benchmarking/m-p/2204321#M991</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254342"&gt;@Cerviik&lt;/a&gt;,&amp;nbsp;&lt;BR /&gt;Great observation. NXP likely ran GFXBench and Antutu on Android builds for the same Arm-based hardware, not native Linux. These benchmarks are Android-compatible and often used to showcase GPU performance even if the target OS for deployment is Linux.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Jill Muncy&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Nov 2025 09:06:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/iMX95-Arm-Mali-G310-GPU-benchmarking/m-p/2204321#M991</guid>
      <dc:creator>jill598muncy</dc:creator>
      <dc:date>2025-11-13T09:06:47Z</dc:date>
    </item>
  </channel>
</rss>