<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX GraphicsのトピックDatasheet of G2D GC520L</title>
    <link>https://community.nxp.com/t5/i-MX-Graphics/Datasheet-of-G2D-GC520L/m-p/2124612#M852</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I am currently working on iMX8 MPlus, and I would like to have the datasheet of the GPU 2D - GC520L. I can't find the actual datasheet anywhere.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The first need of this datasheet is to know the maximum resolution possible for a color conversion.&lt;/P&gt;&lt;P&gt;Also, I would like to know if this GC520L is able to do multiple color conversion at the same time.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Fri, 27 Jun 2025 08:35:55 GMT</pubDate>
    <dc:creator>gaelp</dc:creator>
    <dc:date>2025-06-27T08:35:55Z</dc:date>
    <item>
      <title>Datasheet of G2D GC520L</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/Datasheet-of-G2D-GC520L/m-p/2124612#M852</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I am currently working on iMX8 MPlus, and I would like to have the datasheet of the GPU 2D - GC520L. I can't find the actual datasheet anywhere.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The first need of this datasheet is to know the maximum resolution possible for a color conversion.&lt;/P&gt;&lt;P&gt;Also, I would like to know if this GC520L is able to do multiple color conversion at the same time.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 27 Jun 2025 08:35:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/Datasheet-of-G2D-GC520L/m-p/2124612#M852</guid>
      <dc:creator>gaelp</dc:creator>
      <dc:date>2025-06-27T08:35:55Z</dc:date>
    </item>
    <item>
      <title>Re: Datasheet of G2D GC520L</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/Datasheet-of-G2D-GC520L/m-p/2124818#M853</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You can see all the ip information about GC250L form verisilicon&amp;nbsp;&lt;A href="https://www.chipestimate.com/VeriSilicon/GC520L/datasheet/ip/41812" target="_blank"&gt;https://www.chipestimate.com/VeriSilicon/GC520L/datasheet/ip/41812&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Jun 2025 13:41:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/Datasheet-of-G2D-GC520L/m-p/2124818#M853</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-06-27T13:41:27Z</dc:date>
    </item>
    <item>
      <title>Re: Datasheet of G2D GC520L</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/Datasheet-of-G2D-GC520L/m-p/2124834#M854</link>
      <description>&lt;P&gt;Thank you for your answer.&lt;/P&gt;&lt;P&gt;I have seen this already but it is just an overview of the GC520L and it is a bit succinct.&lt;/P&gt;&lt;P&gt;Anyway, this webpage says that the Resolution support is 1080p, what do you think about that ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Jun 2025 14:01:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/Datasheet-of-G2D-GC520L/m-p/2124834#M854</guid>
      <dc:creator>gaelp</dc:creator>
      <dc:date>2025-06-27T14:01:14Z</dc:date>
    </item>
  </channel>
</rss>