<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX8MM DRM framebuffer does not show splash/logo image during or after kernel boot in i.MX Graphics</title>
    <link>https://community.nxp.com/t5/i-MX-Graphics/i-MX8MM-DRM-framebuffer-does-not-show-splash-logo-image-during/m-p/2106418#M827</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm working on an i.MX8M Mini (i.MX8MM) based board and I'm trying to display a splash screen or any image (even test pattern or static logo) using framebuffer (fb) or DRM/KMS during early boot (kernel stage or just after).&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;U-Boot splash/logo is working fine and shown on display.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;When the kernel boots, the display turns black (screen resets).&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;dmesg shows that imx-drm and fb0 are initialized correctly:&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;/dev/fb0 exists, but writing to it (using tools like fbv, cat, or custom code) does not result in anything on the screen.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Weston works correctly when launched later from the rootfs — it enables the display and rendering works as expected.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;H3&gt;What I've Checked:&lt;/H3&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Kernel has CONFIG_DRM, CONFIG_DRM_IMX, CONFIG_DRM_FBDEV_EMULATION, etc. enabled.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Device Tree has proper lcdif, mipi_dsi, and panel nodes.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Weston runs with drm-backend.so and works well, so the display pipeline is functional.&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;H3&gt;What I want to achieve:&lt;/H3&gt;&lt;P&gt;I want to:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Show a splash screen during or just after kernel boot (before Weston starts).&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Possibly write raw image data directly to framebuffer or use fbv, psplash, or something similar.&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;H3&gt;Questions:&lt;/H3&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;Is there anything specific I should enable in the DRM or IMX DRM driver to get early framebuffer working?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is there a known limitation on imx-drm not supporting fbdev write access until userspace enables the pipeline?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is there an example of using fb0 directly on i.MX8MM DRM to display a raw image without Weston?&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;</description>
    <pubDate>Wed, 28 May 2025 15:45:55 GMT</pubDate>
    <dc:creator>hyilmaz</dc:creator>
    <dc:date>2025-05-28T15:45:55Z</dc:date>
    <item>
      <title>i.MX8MM DRM framebuffer does not show splash/logo image during or after kernel boot</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/i-MX8MM-DRM-framebuffer-does-not-show-splash-logo-image-during/m-p/2106418#M827</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm working on an i.MX8M Mini (i.MX8MM) based board and I'm trying to display a splash screen or any image (even test pattern or static logo) using framebuffer (fb) or DRM/KMS during early boot (kernel stage or just after).&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;U-Boot splash/logo is working fine and shown on display.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;When the kernel boots, the display turns black (screen resets).&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;dmesg shows that imx-drm and fb0 are initialized correctly:&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;/dev/fb0 exists, but writing to it (using tools like fbv, cat, or custom code) does not result in anything on the screen.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Weston works correctly when launched later from the rootfs — it enables the display and rendering works as expected.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;H3&gt;What I've Checked:&lt;/H3&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Kernel has CONFIG_DRM, CONFIG_DRM_IMX, CONFIG_DRM_FBDEV_EMULATION, etc. enabled.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Device Tree has proper lcdif, mipi_dsi, and panel nodes.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Weston runs with drm-backend.so and works well, so the display pipeline is functional.&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;H3&gt;What I want to achieve:&lt;/H3&gt;&lt;P&gt;I want to:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Show a splash screen during or just after kernel boot (before Weston starts).&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Possibly write raw image data directly to framebuffer or use fbv, psplash, or something similar.&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;H3&gt;Questions:&lt;/H3&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;Is there anything specific I should enable in the DRM or IMX DRM driver to get early framebuffer working?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is there a known limitation on imx-drm not supporting fbdev write access until userspace enables the pipeline?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is there an example of using fb0 directly on i.MX8MM DRM to display a raw image without Weston?&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Wed, 28 May 2025 15:45:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/i-MX8MM-DRM-framebuffer-does-not-show-splash-logo-image-during/m-p/2106418#M827</guid>
      <dc:creator>hyilmaz</dc:creator>
      <dc:date>2025-05-28T15:45:55Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MM DRM framebuffer does not show splash/logo image during or after kernel boot</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/i-MX8MM-DRM-framebuffer-does-not-show-splash-logo-image-during/m-p/2111680#M838</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/251015"&gt;@hyilmaz&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;There are some reference solutions for continuous display of logos, please create a SFDC case so that we can share such solutions.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Fri, 06 Jun 2025 01:46:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/i-MX8MM-DRM-framebuffer-does-not-show-splash-logo-image-during/m-p/2111680#M838</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2025-06-06T01:46:22Z</dc:date>
    </item>
  </channel>
</rss>