<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX GraphicsのトピックRe: IMX8MP Vivante Driver Issues</title>
    <link>https://community.nxp.com/t5/i-MX-Graphics/IMX8MP-Vivante-Driver-Issues/m-p/2031630#M714</link>
    <description>&lt;P&gt;Which specific issue was resolved in the latest BSP? I mentioned that I have tested the latest driver so I would like to not have to repeat all the tests.&lt;/P&gt;</description>
    <pubDate>Tue, 21 Jan 2025 17:24:09 GMT</pubDate>
    <dc:creator>alexkl</dc:creator>
    <dc:date>2025-01-21T17:24:09Z</dc:date>
    <item>
      <title>IMX8MP Vivante Driver Issues</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/IMX8MP-Vivante-Driver-Issues/m-p/2029201#M707</link>
      <description>&lt;P&gt;The Vivante driver for the IMX8MP (latest version, version doesn't seem to matter) seems to crash Chromium, crashes in WGPU, and doesn't support EGL_DEFAULT_DISPLAY.&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;nbsp;EGL: Warning: No default display support on wayland&lt;/P&gt;&lt;P&gt;It also throws BadAtttribute when robust access is requested on a GL surface, despite the feature being supported.&lt;/P&gt;&lt;P&gt;1. Is there any plan to support EGL_DEFAULT_DISPLAY on Wayland? Plenty of graphics libraries request the default display.&lt;/P&gt;&lt;P&gt;2. Is there any known issues with Chromium and Vivante? TorizonOS currently does not work on their latest release.&lt;/P&gt;&lt;P&gt;3. WebGL2/WebGPU doesn't appear to work on WGPU-RS based WASM code. It crashes, or is exceptionally slow. Try any of the examples here with a Vivante driver: &lt;A href="https://bevyengine.org/examples/" target="_blank" rel="noopener"&gt;https://bevyengine.org/examples/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;4. Are there any known issues with the driver limitations/stability being worked on for a future release? e.g. robust access&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jan 2025 18:33:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/IMX8MP-Vivante-Driver-Issues/m-p/2029201#M707</guid>
      <dc:creator>alexkl</dc:creator>
      <dc:date>2025-01-16T18:33:37Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP Vivante Driver Issues</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/IMX8MP-Vivante-Driver-Issues/m-p/2029812#M709</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Make sure that you are using the latest BSP:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Since we saw this issue in previous version but now it suppose to be fixed, please check it.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jan 2025 13:44:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/IMX8MP-Vivante-Driver-Issues/m-p/2029812#M709</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-01-17T13:44:30Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP Vivante Driver Issues</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/IMX8MP-Vivante-Driver-Issues/m-p/2031630#M714</link>
      <description>&lt;P&gt;Which specific issue was resolved in the latest BSP? I mentioned that I have tested the latest driver so I would like to not have to repeat all the tests.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jan 2025 17:24:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/IMX8MP-Vivante-Driver-Issues/m-p/2031630#M714</guid>
      <dc:creator>alexkl</dc:creator>
      <dc:date>2025-01-21T17:24:09Z</dc:date>
    </item>
  </channel>
</rss>