<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX GraphicsのトピックRe: I.MX8 LCD display</title>
    <link>https://community.nxp.com/t5/i-MX-Graphics/I-MX8-LCD-display/m-p/2003372#M671</link>
    <description>&lt;P&gt;i.mx8ulp has PXP which can support this feature, refer to the reference manual:&lt;/P&gt;
&lt;P&gt;The PXP module includes following features:&lt;BR /&gt;•&lt;BR /&gt;Scaling&lt;BR /&gt;—&lt;BR /&gt;Supports YUV 422, 420, 444 and any RGB formatted pixels&lt;BR /&gt;—&lt;BR /&gt;The maximum downscaling factor can be up to 16&lt;BR /&gt;•&lt;BR /&gt;Color Space Conversion (CSC)&lt;BR /&gt;—&lt;BR /&gt;Supports converting from YUV to RGB&lt;BR /&gt;—&lt;BR /&gt;Supports bypass mode&lt;BR /&gt;—&lt;BR /&gt;Supports color space coefficients configuration&lt;BR /&gt;•&lt;BR /&gt;Secondary Color Space Conversion (CSC2)&lt;BR /&gt;—&lt;BR /&gt;Supports converting to RGB or YUV color spaces depending on the desired output pixel format&lt;BR /&gt;—&lt;BR /&gt;Supports color space coefficients configuration&lt;/P&gt;
&lt;P&gt;•&lt;BR /&gt;Rotation&lt;BR /&gt;—&lt;BR /&gt;Supports 0, 90, 180, 270 degrees&lt;BR /&gt;—&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;Supports vertical and horizontal flips&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;•&lt;BR /&gt;Composite Alpha Blending and Color Key&lt;BR /&gt;—&lt;BR /&gt;Supports normal alpha blending and Porter-Duff alpha blending.&lt;BR /&gt;—&lt;BR /&gt;Supports color key function to create transparent effects on the output pixel&lt;/P&gt;</description>
    <pubDate>Thu, 28 Nov 2024 05:54:37 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2024-11-28T05:54:37Z</dc:date>
    <item>
      <title>I.MX8 LCD display</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/I-MX8-LCD-display/m-p/2002579#M670</link>
      <description>&lt;P&gt;Does I.mx8PLUS have the ability to flip the LCD display upside down?&lt;/P&gt;</description>
      <pubDate>Wed, 27 Nov 2024 07:09:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/I-MX8-LCD-display/m-p/2002579#M670</guid>
      <dc:creator>SeedsHIRO</dc:creator>
      <dc:date>2024-11-27T07:09:28Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX8 LCD display</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/I-MX8-LCD-display/m-p/2003372#M671</link>
      <description>&lt;P&gt;i.mx8ulp has PXP which can support this feature, refer to the reference manual:&lt;/P&gt;
&lt;P&gt;The PXP module includes following features:&lt;BR /&gt;•&lt;BR /&gt;Scaling&lt;BR /&gt;—&lt;BR /&gt;Supports YUV 422, 420, 444 and any RGB formatted pixels&lt;BR /&gt;—&lt;BR /&gt;The maximum downscaling factor can be up to 16&lt;BR /&gt;•&lt;BR /&gt;Color Space Conversion (CSC)&lt;BR /&gt;—&lt;BR /&gt;Supports converting from YUV to RGB&lt;BR /&gt;—&lt;BR /&gt;Supports bypass mode&lt;BR /&gt;—&lt;BR /&gt;Supports color space coefficients configuration&lt;BR /&gt;•&lt;BR /&gt;Secondary Color Space Conversion (CSC2)&lt;BR /&gt;—&lt;BR /&gt;Supports converting to RGB or YUV color spaces depending on the desired output pixel format&lt;BR /&gt;—&lt;BR /&gt;Supports color space coefficients configuration&lt;/P&gt;
&lt;P&gt;•&lt;BR /&gt;Rotation&lt;BR /&gt;—&lt;BR /&gt;Supports 0, 90, 180, 270 degrees&lt;BR /&gt;—&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;Supports vertical and horizontal flips&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;•&lt;BR /&gt;Composite Alpha Blending and Color Key&lt;BR /&gt;—&lt;BR /&gt;Supports normal alpha blending and Porter-Duff alpha blending.&lt;BR /&gt;—&lt;BR /&gt;Supports color key function to create transparent effects on the output pixel&lt;/P&gt;</description>
      <pubDate>Thu, 28 Nov 2024 05:54:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/I-MX8-LCD-display/m-p/2003372#M671</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2024-11-28T05:54:37Z</dc:date>
    </item>
  </channel>
</rss>