<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX8QM 8-lane MIPI DSI to FPD-Link in i.MX Graphics</title>
    <link>https://community.nxp.com/t5/i-MX-Graphics/iMX8QM-8-lane-MIPI-DSI-to-FPD-Link/m-p/1939308#M613</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;With current device tree you can check two mipi at the time you don't need to change anything.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Fri, 23 Aug 2024 13:53:35 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2024-08-23T13:53:35Z</dc:date>
    <item>
      <title>iMX8QM 8-lane MIPI DSI to FPD-Link</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/iMX8QM-8-lane-MIPI-DSI-to-FPD-Link/m-p/1938615#M612</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I would like to use 2x MIPI DSI ports (8-lanes) to drive a LCD, 4-lanes of odd data, 4-lanes of even data.&amp;nbsp; According to the post in the link below, the iMX8QM does support this.&amp;nbsp; Is there a device tree example of how to achieve this using both DSI ports together?&lt;/P&gt;&lt;P&gt;In the mipi-dsi-bus.txt file in the device tree binding documentation folder, I see this mentioned, but I am unsure how to use this:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Optional properties:
- clock-master: boolean. Should be enabled if the host is being used in
  conjunction with another DSI host to drive the same peripheral. Hardware
  supporting such a configuration generally requires the data on both the busses
  to be driven by the same clock. Only the DSI host instance controlling this
  clock should contain this property.&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Does-mx8-support-8-Lane-Mipi-output/m-p/1076945" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Does-mx8-support-8-Lane-Mipi-output/m-p/1076945&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 22 Aug 2024 16:38:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/iMX8QM-8-lane-MIPI-DSI-to-FPD-Link/m-p/1938615#M612</guid>
      <dc:creator>jsmith8831</dc:creator>
      <dc:date>2024-08-22T16:38:26Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM 8-lane MIPI DSI to FPD-Link</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/iMX8QM-8-lane-MIPI-DSI-to-FPD-Link/m-p/1939308#M613</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;With current device tree you can check two mipi at the time you don't need to change anything.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 23 Aug 2024 13:53:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/iMX8QM-8-lane-MIPI-DSI-to-FPD-Link/m-p/1939308#M613</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-08-23T13:53:35Z</dc:date>
    </item>
  </channel>
</rss>