<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX 6 HDMI Graphic Problem in i.MX Graphics</title>
    <link>https://community.nxp.com/t5/i-MX-Graphics/i-MX-6-HDMI-Graphic-Problem/m-p/1896734#M588</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;compared the mcx_edid.c files and found only two things:&lt;BR /&gt;the first one is the pixel clock for the first element of the video mode (line 44) and the second one is at line 492/493 that sumo has this line of code:index += index_inc;&lt;BR /&gt;I don't know if this cause the problem, another thing that i changed in the dts I've swapped the mxcfb0 and mxcfb1&lt;BR /&gt;&lt;BR /&gt;Thank you,&lt;BR /&gt;Alex&lt;/P&gt;</description>
    <pubDate>Tue, 02 Jul 2024 08:57:41 GMT</pubDate>
    <dc:creator>R_Alex</dc:creator>
    <dc:date>2024-07-02T08:57:41Z</dc:date>
    <item>
      <title>i.MX 6 HDMI Graphic Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/i-MX-6-HDMI-Graphic-Problem/m-p/1895677#M584</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm pretty new to Yocto and I'm updating an old build (sumo) to&amp;nbsp;scarthgap but I'm facing some issues with the HDMI.&lt;/P&gt;&lt;P&gt;As you can see from the attachments the splash screen it's shown correctly but the desktop it's repeated 3 times with tons of vertical lines.&lt;/P&gt;&lt;P&gt;The resolution it's set correctly, I've noticed something strange on the Wayland log that seems to take a refresh rate of 61Hz instead of the 60Hz, fbset return the correct data.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Alex&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 06:22:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/i-MX-6-HDMI-Graphic-Problem/m-p/1895677#M584</guid>
      <dc:creator>R_Alex</dc:creator>
      <dc:date>2024-06-28T06:22:38Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 6 HDMI Graphic Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/i-MX-6-HDMI-Graphic-Problem/m-p/1895990#M586</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Wayland come after the splash screen, check the pixel clock in your old bsp and new one, this can be the cause is not check the entire dtb.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 14:40:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/i-MX-6-HDMI-Graphic-Problem/m-p/1895990#M586</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-06-28T14:40:55Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 6 HDMI Graphic Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/i-MX-6-HDMI-Graphic-Problem/m-p/1896734#M588</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;compared the mcx_edid.c files and found only two things:&lt;BR /&gt;the first one is the pixel clock for the first element of the video mode (line 44) and the second one is at line 492/493 that sumo has this line of code:index += index_inc;&lt;BR /&gt;I don't know if this cause the problem, another thing that i changed in the dts I've swapped the mxcfb0 and mxcfb1&lt;BR /&gt;&lt;BR /&gt;Thank you,&lt;BR /&gt;Alex&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jul 2024 08:57:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/i-MX-6-HDMI-Graphic-Problem/m-p/1896734#M588</guid>
      <dc:creator>R_Alex</dc:creator>
      <dc:date>2024-07-02T08:57:41Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 6 HDMI Graphic Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/i-MX-6-HDMI-Graphic-Problem/m-p/1897420#M589</link>
      <description>&lt;P&gt;I tried applying the changes in the previous message but nothing changes. I've swapped the mxcfb because otherwise I don't have output in the hdmi device even specifing&amp;nbsp;video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jul 2024 10:18:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/i-MX-6-HDMI-Graphic-Problem/m-p/1897420#M589</guid>
      <dc:creator>R_Alex</dc:creator>
      <dc:date>2024-07-02T10:18:30Z</dc:date>
    </item>
  </channel>
</rss>