<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: lunarG sdk is broken so the NXP framework is not useable in i.MX Graphics</title>
    <link>https://community.nxp.com/t5/i-MX-Graphics/lunarG-sdk-is-broken-so-the-NXP-framework-is-not-useable/m-p/1827252#M548</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Which board are you using? since the Mx8 works nicelly but with yocto, you can download the BSP from:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?&amp;amp;&amp;amp;&amp;amp;code=IMXLINUX&amp;amp;" target="_blank"&gt;https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?&amp;amp;&amp;amp;&amp;amp;code=IMXLINUX&amp;amp;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Wed, 13 Mar 2024 14:28:56 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2024-03-13T14:28:56Z</dc:date>
    <item>
      <title>lunarG sdk is broken so the NXP framework is not useable</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/lunarG-sdk-is-broken-so-the-NXP-framework-is-not-useable/m-p/1826599#M547</link>
      <description>&lt;P&gt;We use Ubuntu 22.04 and the lunarG sdk has some issues and will not install so the NXP framework will not work either. Looked it over and tried to grab this and that and try to make it work but that did not work out. My question is what do we do at this point, any suggestions on this.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Mar 2024 22:25:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/lunarG-sdk-is-broken-so-the-NXP-framework-is-not-useable/m-p/1826599#M547</guid>
      <dc:creator>foxsquirrel</dc:creator>
      <dc:date>2024-03-12T22:25:20Z</dc:date>
    </item>
    <item>
      <title>Re: lunarG sdk is broken so the NXP framework is not useable</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/lunarG-sdk-is-broken-so-the-NXP-framework-is-not-useable/m-p/1827252#M548</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Which board are you using? since the Mx8 works nicelly but with yocto, you can download the BSP from:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?&amp;amp;&amp;amp;&amp;amp;code=IMXLINUX&amp;amp;" target="_blank"&gt;https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?&amp;amp;&amp;amp;&amp;amp;code=IMXLINUX&amp;amp;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 13 Mar 2024 14:28:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/lunarG-sdk-is-broken-so-the-NXP-framework-is-not-useable/m-p/1827252#M548</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-03-13T14:28:56Z</dc:date>
    </item>
    <item>
      <title>Re: lunarG sdk is broken so the NXP framework is not useable</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/lunarG-sdk-is-broken-so-the-NXP-framework-is-not-useable/m-p/1827796#M549</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are using Variscite imx8m, imx93, 6ul.&lt;/P&gt;&lt;P&gt;I am using the Varsicte BSP (yocto), was under the assumption it was NXP with some tweaks.&lt;/P&gt;&lt;P&gt;Problem we are having is launching Vulkan and Opengles2.&lt;/P&gt;&lt;P&gt;No problems with Gtk3. Fltk has an issue with the mouse. Touchscreen works fine with Fltk, the cursor disappears when it is in the Fltk screen.&lt;/P&gt;&lt;P&gt;Need to create some application specific graphics and wanted to go with straight wayland and Vulkan.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for the link, was not aware of that information until now.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Fred&lt;/P&gt;</description>
      <pubDate>Thu, 14 Mar 2024 00:18:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/lunarG-sdk-is-broken-so-the-NXP-framework-is-not-useable/m-p/1827796#M549</guid>
      <dc:creator>foxsquirrel</dc:creator>
      <dc:date>2024-03-14T00:18:30Z</dc:date>
    </item>
  </channel>
</rss>