<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic DMA Buf import to Vulkan in i.MX Graphics</title>
    <link>https://community.nxp.com/t5/i-MX-Graphics/DMA-Buf-import-to-Vulkan/m-p/1816887#M532</link>
    <description>&lt;P&gt;I am using an i.MX8M Plus with a MIPI camera. I am writing a compute shader in Vulkan to do video processing. I have a DMA buffer setup which receives the camera frames using V4L2 and the DMA-buf heap protocol. The DMA buffer is in cma-uncached memory. I can memory map this buffer and it appears to be functioning correctly. When I pass the file descriptor to Vulkan, I am unable to get the memory to import. My understanding is that the CPU and GPU share memory so what I am attempting should be possible. Is this correct? Vulkan validation layers do not indicate any problems but the frame data is not imported into my vkBuffer. Any suggestions would be appreciated.&lt;/P&gt;</description>
    <pubDate>Tue, 27 Feb 2024 23:07:33 GMT</pubDate>
    <dc:creator>AB22</dc:creator>
    <dc:date>2024-02-27T23:07:33Z</dc:date>
    <item>
      <title>DMA Buf import to Vulkan</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/DMA-Buf-import-to-Vulkan/m-p/1816887#M532</link>
      <description>&lt;P&gt;I am using an i.MX8M Plus with a MIPI camera. I am writing a compute shader in Vulkan to do video processing. I have a DMA buffer setup which receives the camera frames using V4L2 and the DMA-buf heap protocol. The DMA buffer is in cma-uncached memory. I can memory map this buffer and it appears to be functioning correctly. When I pass the file descriptor to Vulkan, I am unable to get the memory to import. My understanding is that the CPU and GPU share memory so what I am attempting should be possible. Is this correct? Vulkan validation layers do not indicate any problems but the frame data is not imported into my vkBuffer. Any suggestions would be appreciated.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Feb 2024 23:07:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/DMA-Buf-import-to-Vulkan/m-p/1816887#M532</guid>
      <dc:creator>AB22</dc:creator>
      <dc:date>2024-02-27T23:07:33Z</dc:date>
    </item>
    <item>
      <title>Re: DMA Buf import to Vulkan</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/DMA-Buf-import-to-Vulkan/m-p/1818212#M535</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/209988"&gt;@AB22&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I think you may need more debug steps about the data handling process.&lt;/P&gt;
&lt;P&gt;1.Make sure the&amp;nbsp;&lt;SPAN&gt;V4L2&amp;nbsp;driver is working as your want, that frame is stored in memory correctly.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;2.&amp;nbsp;&lt;SPAN&gt;I can memory map this buffer and it appears to be functioning correctly&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;--&amp;gt; Once you check the step1, then check the buffer after mapped.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;3.When I pass the file descriptor to Vulkan, I am unable to get the memory to import&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;--&amp;gt;Firstly, verify dma-buf-import not using VULKAN API. This step is to check if you can dump frame with dma-buf framework.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Zhiming&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 02:19:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/DMA-Buf-import-to-Vulkan/m-p/1818212#M535</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-02-29T02:19:16Z</dc:date>
    </item>
    <item>
      <title>Re: DMA Buf import to Vulkan</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/DMA-Buf-import-to-Vulkan/m-p/1818883#M536</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/151788"&gt;@Zhiming_Liu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Thank you for responding. I should elaborate on my testing.&lt;/P&gt;&lt;P&gt;1. We have used the V4L2 driver with this MIPI camera extensively.&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. After using mmap() with reference to the dma-buf file descriptor, I can memcpy and average a portion of the dma-buf and the values change as I adjust the amount of light reaching the camera.&lt;/P&gt;&lt;P&gt;I will attempt to use the user-space dma-buf commands to import the dma-buf without Vulkan as you suggest.&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 16:37:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/DMA-Buf-import-to-Vulkan/m-p/1818883#M536</guid>
      <dc:creator>AB22</dc:creator>
      <dc:date>2024-02-29T16:37:45Z</dc:date>
    </item>
    <item>
      <title>Re: DMA Buf import to Vulkan</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/DMA-Buf-import-to-Vulkan/m-p/1818916#M537</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/151788"&gt;@Zhiming_Liu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Based on my reading of:&lt;/P&gt;&lt;P&gt;&lt;A href="https://docs.kernel.org/driver-api/dma-buf.html" target="_blank"&gt;https://docs.kernel.org/driver-api/dma-buf.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;In the section entitled, "CPU Access to DMA Buffer Objects". I believe I am correct in using mmap to look at the dma-buf contents. I don't see another user-space command for this purpose. Is there one I am missing?&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 17:38:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/DMA-Buf-import-to-Vulkan/m-p/1818916#M537</guid>
      <dc:creator>AB22</dc:creator>
      <dc:date>2024-02-29T17:38:17Z</dc:date>
    </item>
  </channel>
</rss>