<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX GraphicsのトピックUsing PXP along with VGLite</title>
    <link>https://community.nxp.com/t5/i-MX-Graphics/Using-PXP-along-with-VGLite/m-p/1755230#M494</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Is it possible to use PXP and VGLite at the same time?&lt;BR /&gt;The scenario is:&lt;BR /&gt;1. Build the image using VGLite&lt;BR /&gt;2. Rotate this final image using PXP&lt;/P&gt;&lt;P&gt;Is there some example of how to configure and use them together?&lt;BR /&gt;Or maybe some other solution&lt;BR /&gt;&lt;BR /&gt;The board is MIMXRT1160-EVK&lt;BR /&gt;&lt;BR /&gt;Thank you&lt;/P&gt;</description>
    <pubDate>Fri, 10 Nov 2023 01:06:00 GMT</pubDate>
    <dc:creator>temmka</dc:creator>
    <dc:date>2023-11-10T01:06:00Z</dc:date>
    <item>
      <title>Using PXP along with VGLite</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/Using-PXP-along-with-VGLite/m-p/1755230#M494</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Is it possible to use PXP and VGLite at the same time?&lt;BR /&gt;The scenario is:&lt;BR /&gt;1. Build the image using VGLite&lt;BR /&gt;2. Rotate this final image using PXP&lt;/P&gt;&lt;P&gt;Is there some example of how to configure and use them together?&lt;BR /&gt;Or maybe some other solution&lt;BR /&gt;&lt;BR /&gt;The board is MIMXRT1160-EVK&lt;BR /&gt;&lt;BR /&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Fri, 10 Nov 2023 01:06:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/Using-PXP-along-with-VGLite/m-p/1755230#M494</guid>
      <dc:creator>temmka</dc:creator>
      <dc:date>2023-11-10T01:06:00Z</dc:date>
    </item>
    <item>
      <title>Re: Using PXP along with VGLite</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/Using-PXP-along-with-VGLite/m-p/1755742#M495</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222641"&gt;@temmka&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;In GUI-Guider v1.6.1 GA you could enable both of them and run the simulator without any issues.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Could you please take a look at&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13075.pdf" target="_blank"&gt;AN13075: i.MX RT1170 Heterogeneous Graphics Pipeline – Application Note&lt;/A&gt;? There is mentioned a case when you could use PXP + VGLite implementation.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Kind regards, Raul.&lt;/P&gt;</description>
      <pubDate>Fri, 10 Nov 2023 18:52:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/Using-PXP-along-with-VGLite/m-p/1755742#M495</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2023-11-10T18:52:12Z</dc:date>
    </item>
  </channel>
</rss>