<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Graphics中的主题 HDMI, LVDS two screen logo display problems</title>
    <link>https://community.nxp.com/t5/i-MX-Graphics/HDMI-LVDS-two-screen-logo-display-problems/m-p/1715496#M451</link>
    <description>&lt;P&gt;dear all&lt;/P&gt;&lt;P&gt;Phenomenon：The main screen is lvds interface, resolution is 1980*1080. The secondary screen is HDMI interface, resolution is 1280*1024. When the kernel displays the logo, both screens are displayed by obtaining data from /dev/fb0. Because the resolution is different, the display of the logo always has a screen display position that is wrong.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;I was wondering if there was a way to turn off the HDMI display. Or the two screens use different fb. At present, fb is virtual out of fb_helper in drm framework. I hope to get your help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 01 Sep 2023 03:37:19 GMT</pubDate>
    <dc:creator>chen-wust</dc:creator>
    <dc:date>2023-09-01T03:37:19Z</dc:date>
    <item>
      <title>HDMI, LVDS two screen logo display problems</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/HDMI-LVDS-two-screen-logo-display-problems/m-p/1715496#M451</link>
      <description>&lt;P&gt;dear all&lt;/P&gt;&lt;P&gt;Phenomenon：The main screen is lvds interface, resolution is 1980*1080. The secondary screen is HDMI interface, resolution is 1280*1024. When the kernel displays the logo, both screens are displayed by obtaining data from /dev/fb0. Because the resolution is different, the display of the logo always has a screen display position that is wrong.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;I was wondering if there was a way to turn off the HDMI display. Or the two screens use different fb. At present, fb is virtual out of fb_helper in drm framework. I hope to get your help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Sep 2023 03:37:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/HDMI-LVDS-two-screen-logo-display-problems/m-p/1715496#M451</guid>
      <dc:creator>chen-wust</dc:creator>
      <dc:date>2023-09-01T03:37:19Z</dc:date>
    </item>
    <item>
      <title>Re: HDMI, LVDS two screen logo display problems</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/HDMI-LVDS-two-screen-logo-display-problems/m-p/1743797#M477</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello, I had the same problem. Have you solved this problem? Thanks.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 20 Oct 2023 15:44:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/HDMI-LVDS-two-screen-logo-display-problems/m-p/1743797#M477</guid>
      <dc:creator>Letu</dc:creator>
      <dc:date>2023-10-20T15:44:38Z</dc:date>
    </item>
  </channel>
</rss>