<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX GraphicsのトピックShader Compile Best Practices</title>
    <link>https://community.nxp.com/t5/i-MX-Graphics/Shader-Compile-Best-Practices/m-p/1457355#M292</link>
    <description>&lt;P&gt;Trying to understand the best practice for compiling shaders on IMX8 Plus. Using function &lt;EM&gt;glCompileShader&lt;/EM&gt; and &lt;EM&gt;glLinkProgram &lt;/EM&gt;seems to produce really slow shader code.&amp;nbsp; Pre-compiling with Vivante IDE produced code that was 2x-3x as fast.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a way to configure the system so that run-time compiled code is as efficient as code compiled with IDE.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the IDE the target hardware is a configuration parameter to vCompiler.exe but I can't find similar configuration of any kind on the system?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 12 May 2022 15:13:03 GMT</pubDate>
    <dc:creator>_Alex_</dc:creator>
    <dc:date>2022-05-12T15:13:03Z</dc:date>
    <item>
      <title>Shader Compile Best Practices</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/Shader-Compile-Best-Practices/m-p/1457355#M292</link>
      <description>&lt;P&gt;Trying to understand the best practice for compiling shaders on IMX8 Plus. Using function &lt;EM&gt;glCompileShader&lt;/EM&gt; and &lt;EM&gt;glLinkProgram &lt;/EM&gt;seems to produce really slow shader code.&amp;nbsp; Pre-compiling with Vivante IDE produced code that was 2x-3x as fast.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a way to configure the system so that run-time compiled code is as efficient as code compiled with IDE.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the IDE the target hardware is a configuration parameter to vCompiler.exe but I can't find similar configuration of any kind on the system?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 12 May 2022 15:13:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/Shader-Compile-Best-Practices/m-p/1457355#M292</guid>
      <dc:creator>_Alex_</dc:creator>
      <dc:date>2022-05-12T15:13:03Z</dc:date>
    </item>
  </channel>
</rss>