<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Graphicsのトピックi.MX6 Color Correction</title>
    <link>https://community.nxp.com/t5/i-MX-Graphics/i-MX6-Color-Correction/m-p/1437695#M287</link>
    <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;currently I'm working on a custom i.MX6DL Board wih Mainline Linux-Kernel.&lt;BR /&gt;But the display attached to it does need some color-correctien (red seems more like orange).&lt;BR /&gt;The Display is a small RGB-Display, so no LDB is used.&lt;/P&gt;&lt;P&gt;I know that the IPU is capable of doing that, but it seems, that the Mainline-Kernel doesn't support it. So I want to switch to the Community-Kernel, but I'm having some problems.&lt;BR /&gt;I managed to boot the Community-Kernel, but it doesn't show anything on the display.&lt;/P&gt;&lt;P&gt;Also it's lacking the /dev/fb* Devices and /dev/dri/card1&lt;/P&gt;&lt;P&gt;I checked it on SabreSD, too. Mainline Kernel shows Tux and a Command-Line via HDMI, Community-Kernel doesn't, although there are four /dev/fb* (but also no /dev/dri/card1).&lt;/P&gt;&lt;P&gt;I know it must be a Devicetree-Issue, but I'm not sure where to get the right hints for this.&lt;/P&gt;&lt;P&gt;Are there any Devicetree snippets available out there?&lt;BR /&gt;Do you need more details?&lt;/P&gt;&lt;P&gt;Greetings&lt;BR /&gt;Steffen&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 01 Apr 2022 13:28:20 GMT</pubDate>
    <dc:creator>steffendoster</dc:creator>
    <dc:date>2022-04-01T13:28:20Z</dc:date>
    <item>
      <title>i.MX6 Color Correction</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/i-MX6-Color-Correction/m-p/1437695#M287</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;currently I'm working on a custom i.MX6DL Board wih Mainline Linux-Kernel.&lt;BR /&gt;But the display attached to it does need some color-correctien (red seems more like orange).&lt;BR /&gt;The Display is a small RGB-Display, so no LDB is used.&lt;/P&gt;&lt;P&gt;I know that the IPU is capable of doing that, but it seems, that the Mainline-Kernel doesn't support it. So I want to switch to the Community-Kernel, but I'm having some problems.&lt;BR /&gt;I managed to boot the Community-Kernel, but it doesn't show anything on the display.&lt;/P&gt;&lt;P&gt;Also it's lacking the /dev/fb* Devices and /dev/dri/card1&lt;/P&gt;&lt;P&gt;I checked it on SabreSD, too. Mainline Kernel shows Tux and a Command-Line via HDMI, Community-Kernel doesn't, although there are four /dev/fb* (but also no /dev/dri/card1).&lt;/P&gt;&lt;P&gt;I know it must be a Devicetree-Issue, but I'm not sure where to get the right hints for this.&lt;/P&gt;&lt;P&gt;Are there any Devicetree snippets available out there?&lt;BR /&gt;Do you need more details?&lt;/P&gt;&lt;P&gt;Greetings&lt;BR /&gt;Steffen&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Apr 2022 13:28:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/i-MX6-Color-Correction/m-p/1437695#M287</guid>
      <dc:creator>steffendoster</dc:creator>
      <dc:date>2022-04-01T13:28:20Z</dc:date>
    </item>
  </channel>
</rss>