<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX GraphicsのトピックRe: iMX8M Plus VPU max fps</title>
    <link>https://community.nxp.com/t5/i-MX-Graphics/iMX8M-Plus-VPU-max-fps/m-p/1367374#M223</link>
    <description>&lt;P&gt;The values I'm referring to are the output of the test_enc_arm_elinux script (see attached photo)&lt;/P&gt;</description>
    <pubDate>Fri, 05 Nov 2021 14:11:40 GMT</pubDate>
    <dc:creator>gawarren</dc:creator>
    <dc:date>2021-11-05T14:11:40Z</dc:date>
    <item>
      <title>iMX8M Plus VPU max fps</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/iMX8M-Plus-VPU-max-fps/m-p/1366925#M221</link>
      <description>&lt;P&gt;According to the reference manual, the iMX8M Plus is capable of h264/5 encoding with image resolution 1920x1080 at 60 Hz. I would like to know under what conditions this framerate is acheivable? Is this for full color input YUV444? Should I achieve a higher fps with less input, such as YUV420?&lt;/P&gt;&lt;P&gt;I am using the vpuwrap library and YUV420 input format. Depending on my quantization settings, I am getting above 100 fps (for high QP values) and below 60 fps (for low QP values). Is it possible to get above 60 fps, or is this an inaccuracy in the timing?&lt;/P&gt;</description>
      <pubDate>Thu, 04 Nov 2021 20:27:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/iMX8M-Plus-VPU-max-fps/m-p/1366925#M221</guid>
      <dc:creator>gawarren</dc:creator>
      <dc:date>2021-11-04T20:27:50Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Plus VPU max fps</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/iMX8M-Plus-VPU-max-fps/m-p/1367253#M222</link>
      <description>&lt;P&gt;Actual maximum bit rate and frame rate will depend on the logic clock frequency and the system bus performance. for imx8mp encoding, which can support h.264 up to &lt;A href="mailto:1080p@60" target="_blank"&gt;1080p@60&lt;/A&gt; frame rate (40Mbps), for H.265, up to 1920x1080 with 60 frame rate, as I known, the swreg fixed the 1080p as the max resolution, couldn't support 4k, the 60fps we talking about this encoding time/total time(including pipeline run time), if you mean core encoding fps, maybe you can get more than 60fps&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Nov 2021 09:21:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/iMX8M-Plus-VPU-max-fps/m-p/1367253#M222</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-11-05T09:21:13Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Plus VPU max fps</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/iMX8M-Plus-VPU-max-fps/m-p/1367374#M223</link>
      <description>&lt;P&gt;The values I'm referring to are the output of the test_enc_arm_elinux script (see attached photo)&lt;/P&gt;</description>
      <pubDate>Fri, 05 Nov 2021 14:11:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/iMX8M-Plus-VPU-max-fps/m-p/1367374#M223</guid>
      <dc:creator>gawarren</dc:creator>
      <dc:date>2021-11-05T14:11:40Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Plus VPU max fps</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/iMX8M-Plus-VPU-max-fps/m-p/1369112#M224</link>
      <description>&lt;P&gt;as I mentioned before, the value you test should be core encoding frame rate, if you mean core encoding value, the max frame rate can up to 200 fps&lt;/P&gt;</description>
      <pubDate>Wed, 10 Nov 2021 08:34:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/iMX8M-Plus-VPU-max-fps/m-p/1369112#M224</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-11-10T08:34:33Z</dc:date>
    </item>
  </channel>
</rss>