<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX GraphicsのトピックRe: IMX8mp mipi dsi in command mode</title>
    <link>https://community.nxp.com/t5/i-MX-Graphics/IMX8mp-mipi-dsi-in-command-mode/m-p/2302259#M1035</link>
    <description>&lt;P&gt;If I follow the guide for command mode, the mipi interface dose not send out any data to the display, only when using video mode.&lt;/P&gt;&lt;P&gt;There is a samsung driver that implement support for IMX8MP (samsung-dsim.c).&lt;/P&gt;&lt;P&gt;Is that a better&amp;nbsp;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;choices&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&amp;nbsp;when using command mode?&lt;/P&gt;</description>
    <pubDate>Wed, 28 Jan 2026 12:38:39 GMT</pubDate>
    <dc:creator>persandberg</dc:creator>
    <dc:date>2026-01-28T12:38:39Z</dc:date>
    <item>
      <title>IMX8mp mipi dsi in command mode</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/IMX8mp-mipi-dsi-in-command-mode/m-p/2252349#M998</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have a cutom board with iMX8MP and a AMOLED display with a CH13721C controller. We have video mode working but would like to use command mode and use the internal frame buffer in the display controller to show a static image on the display.&lt;BR /&gt;From the reference manual of iMX8mp in table 13-26 a initialization sequence is described of how to get command mode woring but I can not get it to work. I can also not find a Linux driver that fully utilyze the command mode.&lt;BR /&gt;Any help is much appreciated.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Skärmbild 2025-12-01 152150.png" style="width: 602px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/368023i4ADC9ED1108F29AE/image-size/large?v=v2&amp;amp;px=999" role="button" title="Skärmbild 2025-12-01 152150.png" alt="Skärmbild 2025-12-01 152150.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Dec 2025 14:22:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/IMX8mp-mipi-dsi-in-command-mode/m-p/2252349#M998</guid>
      <dc:creator>persandberg</dc:creator>
      <dc:date>2025-12-01T14:22:48Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8mp mipi dsi in command mode</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/IMX8mp-mipi-dsi-in-command-mode/m-p/2254523#M999</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;For this you may refer to the Linux driver:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.12.y/drivers/video/fbdev/mxc/mipi_dsi.c#L472" target="_blank"&gt;https://github.com/nxp-imx/linux-imx/blob/lf-6.12.y/drivers/video/fbdev/mxc/mipi_dsi.c#L472&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Wed, 03 Dec 2025 21:35:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/IMX8mp-mipi-dsi-in-command-mode/m-p/2254523#M999</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2025-12-03T21:35:26Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8mp mipi dsi in command mode</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/IMX8mp-mipi-dsi-in-command-mode/m-p/2257236#M1000</link>
      <description>&lt;P&gt;Thanks for responding!&lt;/P&gt;&lt;P&gt;Are the registers used in mipi_dsi.c the same as the ones in iMX8MP?&lt;/P&gt;&lt;P&gt;Have I understand it correctlly that the internal bus (S-i80) in the CPU writes to the FIFO if command mode is activated by setting bit 31 in&amp;nbsp;DSIM_RGB_STATUS?&lt;/P&gt;&lt;P&gt;Pleas let me know if you need more information.&lt;/P&gt;</description>
      <pubDate>Mon, 08 Dec 2025 14:30:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/IMX8mp-mipi-dsi-in-command-mode/m-p/2257236#M1000</guid>
      <dc:creator>persandberg</dc:creator>
      <dc:date>2025-12-08T14:30:04Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8mp mipi dsi in command mode</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/IMX8mp-mipi-dsi-in-command-mode/m-p/2291586#M1011</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I understand it correctly thanks so much share this correct guidance.&lt;/P&gt;</description>
      <pubDate>Mon, 12 Jan 2026 08:49:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/IMX8mp-mipi-dsi-in-command-mode/m-p/2291586#M1011</guid>
      <dc:creator>jerrymarlowe45</dc:creator>
      <dc:date>2026-01-12T08:49:47Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8mp mipi dsi in command mode</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/IMX8mp-mipi-dsi-in-command-mode/m-p/2292644#M1013</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is that implementation rellay for theiMX8MP processor?&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jan 2026 14:25:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/IMX8mp-mipi-dsi-in-command-mode/m-p/2292644#M1013</guid>
      <dc:creator>persandberg</dc:creator>
      <dc:date>2026-01-13T14:25:05Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8mp mipi dsi in command mode</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/IMX8mp-mipi-dsi-in-command-mode/m-p/2297492#M1027</link>
      <description>&lt;P&gt;I am unable to figure out how to configure command mode for the IMX8MP processor.&lt;/P&gt;&lt;P&gt;If bit 25 (Video mode) is cleared in register DSI_CONFIG and bit 31 is set in register DSI_MDRESOL, nothing is transfered from the fifo, not even commands to the display. If i clear bit 31, I can send commands but no image data is transfered.&lt;BR /&gt;Please&amp;nbsp; help&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jan 2026 15:42:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/IMX8mp-mipi-dsi-in-command-mode/m-p/2297492#M1027</guid>
      <dc:creator>persandberg</dc:creator>
      <dc:date>2026-01-21T15:42:44Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8mp mipi dsi in command mode</title>
      <link>https://community.nxp.com/t5/i-MX-Graphics/IMX8mp-mipi-dsi-in-command-mode/m-p/2302259#M1035</link>
      <description>&lt;P&gt;If I follow the guide for command mode, the mipi interface dose not send out any data to the display, only when using video mode.&lt;/P&gt;&lt;P&gt;There is a samsung driver that implement support for IMX8MP (samsung-dsim.c).&lt;/P&gt;&lt;P&gt;Is that a better&amp;nbsp;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;choices&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&amp;nbsp;when using command mode?&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jan 2026 12:38:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Graphics/IMX8mp-mipi-dsi-in-command-mode/m-p/2302259#M1035</guid>
      <dc:creator>persandberg</dc:creator>
      <dc:date>2026-01-28T12:38:39Z</dc:date>
    </item>
  </channel>
</rss>