<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>HoverGames Drone ChallengeのトピックStuck on tutorial HG-PX4 Example Lab 3: Building Code</title>
    <link>https://community.nxp.com/t5/HoverGames-Drone-Challenge/Stuck-on-tutorial-HG-PX4-Example-Lab-3-Building-Code/m-p/1774172#M189</link>
    <description>&lt;P&gt;Im following your tutorial to build code for PX4&lt;/P&gt;&lt;P&gt;On the third tutorial (&lt;A href="https://nxp.gitbook.io/hovergames/developerguide/px4-tutorial-example-code/hg-px4-example-lab-3" target="_blank" rel="noopener"&gt;https://nxp.gitbook.io/hovergames/developerguide/px4-tutorial-example-code/hg-px4-example-lab-3&lt;/A&gt;), it says:&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Navigate to Firmware/boards/nxp/fmuk66-v3/default.cmake&lt;/SPAN&gt; and&lt;SPAN&gt; add hg_led to the list under EXAMPLES.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;But there is no cmake file in that folder of the PX4 repository I cloned.&lt;/P&gt;&lt;P&gt;The only files in that folder are:&lt;/P&gt;&lt;P&gt;default.px4board&lt;/P&gt;&lt;P&gt;firmware.prototype&lt;/P&gt;&lt;P&gt;socketcan.px4board&lt;/P&gt;&lt;P&gt;test.px4board&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do I add the hg_led application to PX4 firmware without that file?&lt;/P&gt;</description>
    <pubDate>Wed, 13 Dec 2023 20:14:01 GMT</pubDate>
    <dc:creator>hal2</dc:creator>
    <dc:date>2023-12-13T20:14:01Z</dc:date>
    <item>
      <title>Stuck on tutorial HG-PX4 Example Lab 3: Building Code</title>
      <link>https://community.nxp.com/t5/HoverGames-Drone-Challenge/Stuck-on-tutorial-HG-PX4-Example-Lab-3-Building-Code/m-p/1774172#M189</link>
      <description>&lt;P&gt;Im following your tutorial to build code for PX4&lt;/P&gt;&lt;P&gt;On the third tutorial (&lt;A href="https://nxp.gitbook.io/hovergames/developerguide/px4-tutorial-example-code/hg-px4-example-lab-3" target="_blank" rel="noopener"&gt;https://nxp.gitbook.io/hovergames/developerguide/px4-tutorial-example-code/hg-px4-example-lab-3&lt;/A&gt;), it says:&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Navigate to Firmware/boards/nxp/fmuk66-v3/default.cmake&lt;/SPAN&gt; and&lt;SPAN&gt; add hg_led to the list under EXAMPLES.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;But there is no cmake file in that folder of the PX4 repository I cloned.&lt;/P&gt;&lt;P&gt;The only files in that folder are:&lt;/P&gt;&lt;P&gt;default.px4board&lt;/P&gt;&lt;P&gt;firmware.prototype&lt;/P&gt;&lt;P&gt;socketcan.px4board&lt;/P&gt;&lt;P&gt;test.px4board&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do I add the hg_led application to PX4 firmware without that file?&lt;/P&gt;</description>
      <pubDate>Wed, 13 Dec 2023 20:14:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/HoverGames-Drone-Challenge/Stuck-on-tutorial-HG-PX4-Example-Lab-3-Building-Code/m-p/1774172#M189</guid>
      <dc:creator>hal2</dc:creator>
      <dc:date>2023-12-13T20:14:01Z</dc:date>
    </item>
  </channel>
</rss>