<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>HoverGames Drone ChallengeのトピックRe: FMU broken - cannot erase or program</title>
    <link>https://community.nxp.com/t5/HoverGames-Drone-Challenge/FMU-broken-cannot-erase-or-program/m-p/1610912#M184</link>
    <description>&lt;P&gt;Summary - Normally for the FMU there is a bootloader file written to 0x0000 and then a program file at 0x6000.&amp;nbsp; It is believed that the program file was accidentally written to 0x6000 AND that this particular compilation did coincidentally have the security bits flashed.&lt;BR /&gt;The unlocking may not have worked in this instance:&lt;BR /&gt;&lt;A href="https://forum.segger.com/index.php/Thread/2390-JLink-on-unsecure-and-erase-Kinetis-FLASH/" target="_blank"&gt;https://forum.segger.com/index.php/Thread/2390-JLink-on-unsecure-and-erase-Kinetis-FLASH/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 07 Mar 2023 12:44:40 GMT</pubDate>
    <dc:creator>iaingalloway</dc:creator>
    <dc:date>2023-03-07T12:44:40Z</dc:date>
    <item>
      <title>FMU broken - cannot erase or program</title>
      <link>https://community.nxp.com/t5/HoverGames-Drone-Challenge/FMU-broken-cannot-erase-or-program/m-p/1586841#M182</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to erase the FMU board that came on the HoverGames3 kit and I am getting issues of protected device and J-Link or J-Flash both fails.&lt;/P&gt;&lt;P&gt;The original post is &lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/cannot-program-FMU-board-using-SWD-J-Link-cannot-unlock-device/m-p/1582768#M64580" target="_self"&gt;here&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Trying with J-Flash also fails as shown in the attachment .Segger can read the whole device no problem and comms seems ok.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using J-Link PLUS with J-Flash as the little mini edu thing won't have the license to use with it.&lt;/P&gt;&lt;P&gt;What could be wrong?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 23 Jan 2023 21:56:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/HoverGames-Drone-Challenge/FMU-broken-cannot-erase-or-program/m-p/1586841#M182</guid>
      <dc:creator>manuel_iglesias</dc:creator>
      <dc:date>2023-01-23T21:56:39Z</dc:date>
    </item>
    <item>
      <title>Re: FMU broken - cannot erase or program</title>
      <link>https://community.nxp.com/t5/HoverGames-Drone-Challenge/FMU-broken-cannot-erase-or-program/m-p/1588363#M183</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;have you tried flashing the firmware using the QGroundControl Software (&lt;A href="https://nxp.gitbook.io/hovergames/userguide/qgroundcontrol/firmware" target="_blank"&gt;Firmware - NXP HoverGames (gitbook.io)&lt;/A&gt;) ?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I also built the Bootloader myself following this part of our documentation:&amp;nbsp;&lt;A href="https://nxp.gitbook.io/hovergames/developerguide/building-bootloader" target="_blank"&gt;Building the bootloader - NXP HoverGames (gitbook.io)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Might I also invite you to come join the Hackster Discord Server, where many of the discussions around HoverGames are taking place:&amp;nbsp;&lt;A class="anchor-1MIwyf anchorUnderlineOnHover-2qPutX" tabindex="0" title="https://discord.gg/3bcCEYTFz7" role="button" href="https://discord.gg/3bcCEYTFz7" target="_blank" rel="noreferrer noopener"&gt;https://discord.gg/3bcCEYTFz7&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Kind Regards&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Amar&lt;/P&gt;</description>
      <pubDate>Thu, 26 Jan 2023 14:58:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/HoverGames-Drone-Challenge/FMU-broken-cannot-erase-or-program/m-p/1588363#M183</guid>
      <dc:creator>NXPAmar</dc:creator>
      <dc:date>2023-01-26T14:58:00Z</dc:date>
    </item>
    <item>
      <title>Re: FMU broken - cannot erase or program</title>
      <link>https://community.nxp.com/t5/HoverGames-Drone-Challenge/FMU-broken-cannot-erase-or-program/m-p/1610912#M184</link>
      <description>&lt;P&gt;Summary - Normally for the FMU there is a bootloader file written to 0x0000 and then a program file at 0x6000.&amp;nbsp; It is believed that the program file was accidentally written to 0x6000 AND that this particular compilation did coincidentally have the security bits flashed.&lt;BR /&gt;The unlocking may not have worked in this instance:&lt;BR /&gt;&lt;A href="https://forum.segger.com/index.php/Thread/2390-JLink-on-unsecure-and-erase-Kinetis-FLASH/" target="_blank"&gt;https://forum.segger.com/index.php/Thread/2390-JLink-on-unsecure-and-erase-Kinetis-FLASH/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Mar 2023 12:44:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/HoverGames-Drone-Challenge/FMU-broken-cannot-erase-or-program/m-p/1610912#M184</guid>
      <dc:creator>iaingalloway</dc:creator>
      <dc:date>2023-03-07T12:44:40Z</dc:date>
    </item>
  </channel>
</rss>